![]() |
Maestro Audio Framework v 1.5
NXP Semiconductors
|
#include <streamer.h>
Data Fields | |
| ElementHandle | src_element |
| Element handle of msg source. | |
| uint32_t | message |
| Message type. | |
| uintptr_t | data |
| Message data. | |
StreamMessage structure. Pipeline elements will communicate with the application using this message format. All msgs are defined in streamer_message.h