![]() |
Maestro Audio Framework v 1.5
NXP Semiconductors
|
VIT sink element's data structure. More...
#include <vit_sink.h>
Data Fields | |
| int32_t(* | change_state )(struct _StreamElement *, PipelineState) |
| Change state function pointer. | |
| int32_t(* | set_property )(struct _StreamElement *, uint16_t prop, uint32_t val) |
| Set property function pointer. | |
| int32_t(* | get_property )(struct _StreamElement *, uint16_t prop, uint32_t *val_ptr) |
| Get property function pointer. | |
| void * | parent |
| Parent pointer. | |
| int8_t | key |
| Key. | |
| int8_t | depth |
| Depth. | |
| PipelineState | state |
| Pipeline state. | |
| StreamElementType | type |
| Element type. | |
| PadSrc | src_pad [MAX_NUM_PADS] |
| Source pads. | |
| PadSink | sink_pad [MAX_NUM_PADS] |
| Sink pads. | |
| struct _StreamElement * | sibling |
| Sibling pointer. | |
| char * | location |
| pointer to memory buffer start address | |
| uint8_t | raw_write |
| raw write mode | |
| uint32_t | size |
| memory buffer size | |
| uint32_t | current_index |
| internal used for memory buffer | |
| VitSinkInitFunc | init_func |
| Init function pointer. | |
| VitSinkPostProcFunc | proc_func |
| Process function pointer. | |
| VitSinkDeinitFunc | deinit_func |
| Deinit function pointer. | |
| void * | arg_ptr |
| Arguments pointer. | |
| bool | initialized |
| Initialized flag. | |
This data structure is created by create_element, initialized by vitsink_init_element