![]() |
Maestro Audio Framework v 1.5
NXP Semiconductors
|
This structure is used by the decoder to register the callback APIs.
#include <ccidec.h>
Data Fields | |
| pfnReadCallback * | pfnRead |
| Pointer to a function that Reads data from the input stream. | |
| pfnSeekCallback * | pfnSeek |
| Pointer to a function that seeks the input stream. | |
| pfnFtellCallback * | pfnFtell |
| Pointer to a function that gives current position of the input stream. | |