![]() |
Maestro Audio Framework v 1.5
NXP Semiconductors
|
#include <streamer_api.h>
Data Fields | |
| uint32_t | value32u |
| 32 bit unsigned value | |
| uint16_t | value16u |
| 16 bit unsigned value | |
| uint8_t | value8u |
| 8 bit unsigned value | |
| int32_t | value32s |
| 32 bit signed value | |
| int16_t | value16s |
| 16 bit signed value | |
| int8_t | value8s |
| 8 bit signed value | |
| uint8_t | valuebool |
| bool value | |
| StreamStringType | string |
| string value | |
| StreamImageType | image |
| image value | |
Holds the data related to a query or event