![]() |
eRPC API Reference
Rev. 1.11.0
NXP Semiconductors
|
This is the complete list of members for erpc::RequestContext, including all inherited members.
| getCodec(void) | erpc::RequestContext | inline |
| getSequence(void) const | erpc::RequestContext | inline |
| isOneway(void) const | erpc::RequestContext | inline |
| m_codec | erpc::RequestContext | protected |
| m_oneway | erpc::RequestContext | protected |
| m_sequence | erpc::RequestContext | protected |
| RequestContext(uint32_t sequence, Codec *codec, bool argIsOneway) | erpc::RequestContext | inline |
| setIsOneway(bool oneway) | erpc::RequestContext | inline |