![]() |
eRPC Generator (erpcgen)
Rev. 1.11.0
NXP Semiconductors
|
Represents the builtin atomic types. More...
#include <BuiltinType.hpp>
Public Types | |
| enum | _builtin_type { kBoolType, kInt8Type, kInt16Type, kInt32Type, kInt64Type, kUInt8Type, kUInt16Type, kUInt32Type, kUInt64Type, kFloatType, kDoubleType, kStringType, kUStringType, kBinaryType } |
| Atomic builtin types. | |
Public Types inherited from erpcgen::DataType | |
| enum | data_type_t { kAliasType, kArrayType, kBuiltinType, kEnumType, kFunctionType, kListType, kStructType, kUnionType, kVoidType } |
| Supported data types. | |
Public Types inherited from erpcgen::Symbol | |
| enum | symbol_type_t { kConstSymbol, kEnumMemberSymbol, kFunctionSymbol, kInterfaceSymbol, kProgramSymbol, kStructMemberSymbol, kTypenameSymbol, kUnionCaseMemberSymbol } |
| Supported symbol types. | |
Public Member Functions | |
| BuiltinType (const std::string &name, _builtin_type builtinType) | |
| Constructor. More... | |
| _builtin_type | getBuiltinType () const |
| This function returns builtin type. More... | |
| virtual bool | isScalar () const override |
| This function return "true" value for identify scalar type. More... | |
| virtual bool | isInt () const override |
| This function return "true" value for identify int type. More... | |
| virtual bool | isFloat () const override |
| This function return "true" value for identify float type. More... | |
| virtual bool | isBool () const override |
| This function return "true" value for identify bool type. More... | |
| virtual bool | isString () const override |
| This function return true/false value for identify string type. More... | |
| virtual bool | isUString () const override |
| This function return true/false value for identify ustring type. More... | |
| virtual bool | isBinary () const override |
| This function return true/false value for identify binary type. More... | |
Public Member Functions inherited from erpcgen::DataType | |
| DataType (data_type_t dataType) | |
| Constructor. More... | |
| DataType (const std::string &name, data_type_t dataType) | |
| Constructor. More... | |
| DataType (const Token &tok, data_type_t dataType) | |
| Constructor. More... | |
| data_type_t | getDataType () const |
| This function returns data type. More... | |
| DataType * | getTrueDataType () |
| This function returns pointer to true data type instead of alias. More... | |
| DataType * | getTrueContainerDataType () |
| This function returns pointer to true data type (enum, builtin, structs) except lists and arrays. More... | |
| bool | isAlias () const |
| This function is testing data type. More... | |
| bool | isArray () const |
| This function is testing data type. More... | |
| bool | isBuiltin () const |
| This function is testing data type. More... | |
| bool | isEnum () const |
| This function is testing data type. More... | |
| bool | isFunction () const |
| This function is testing data type. More... | |
| bool | isList () const |
| This function is testing data type. More... | |
| bool | isStruct () const |
| This function is testing data type. More... | |
| bool | isUnion () const |
| This function is testing data type. More... | |
| bool | isVoid () const |
| This function is testing data type. More... | |
Public Member Functions inherited from erpcgen::Symbol | |
| Symbol (symbol_type_t symType) | |
| Constructor. More... | |
| Symbol (symbol_type_t symType, const std::string &name) | |
| Constructor. More... | |
| Symbol (symbol_type_t symType, const Token &tok) | |
| Constructor. More... | |
| virtual | ~Symbol () |
| Destructor. | |
| symbol_type_t | getSymbolType () const |
| This function returns symbol type. More... | |
| const std::string & | getName () const |
| This function returns symbol name. More... | |
| void | setName (const std::string &newName) |
| This function set symbol name. More... | |
| bool | isConstSymbol () const |
| This function is testing symbol type. More... | |
| bool | isEnumMemberSymbol () const |
| This function is testing symbol type. More... | |
| bool | isFunctionSymbol () const |
| This function is testing symbol type. More... | |
| bool | isInterfaceSymbol () const |
| This function is testing symbol type. More... | |
| bool | isProgramSymbol () const |
| This function is testing symbol type. More... | |
| bool | isStructMemberSymbol () const |
| This function is testing symbol type. More... | |
| bool | isDatatypeSymbol () const |
| This function is testing symbol type. More... | |
| bool | isUnionCaseSymbol () const |
| This function is testing symbol type. More... | |
| token_loc_t & | getLocation () |
| This function returns location for symbol. More... | |
| void | setLocation (const token_loc_t &loc) |
| This function set location for symbol. More... | |
| int | getFirstLine () const |
| This function return first line from location of symbol. More... | |
| int | getLastLine () const |
| This function return last line from location of symbol. More... | |
| virtual std::string | getDescription () const |
| This function returns description about the symbol (symbol name). More... | |
| void | addAnnotation (const Annotation &a) |
| This function add annotation to vector of symbol annotations. More... | |
| std::string | printAnnotations () |
| This function returns description about annotation. More... | |
| Annotation * | findAnnotation (const std::string &name, Annotation::program_lang_t lang) |
| Find annotation in the annotation list. More... | |
| std::vector< Annotation * > | getAnnotations (const std::string &name, Annotation::program_lang_t lang) |
| Find annotations matching name in the annotation list. More... | |
| const std::vector< Annotation > & | getAnnotations () const |
| Return all Symbol annotations. More... | |
| Value * | getAnnValue (const std::string &annName, Annotation::program_lang_t lang) |
| This function search and returns Value object for given annotation name. More... | |
| std::string | getAnnStringValue (const std::string &annName, Annotation::program_lang_t lang) |
| This function search and returns string for given annotation name. More... | |
| std::string | getMlComment () |
| This function returns multiline comment for this symbol declared in IDL file. More... | |
| void | setMlComment (const std::string &comment) |
| This function set multiline comment for this symbol declared in IDL file. More... | |
| std::string | getIlComment () |
| This function returns inline comment for this symbol declared in IDL file. More... | |
| void | setIlComment (const std::string &comment) |
| This function set inline comment for this symbol declared in IDL file. More... | |
Protected Attributes | |
| _builtin_type | m_builtinType |
Protected Attributes inherited from erpcgen::DataType | |
| data_type_t | m_dataType |
Protected Attributes inherited from erpcgen::Symbol | |
| symbol_type_t | m_symbolType |
| std::string | m_name |
| token_loc_t | m_location |
| std::vector< Annotation > | m_annotations |
| std::string | m_mlComment |
| std::string | m_ilComment |
Represents the builtin atomic types.
|
inline |
Constructor.
This function set builtin type to given builtin type and name to given name.
| [in] | name | Given name. |
| [in] | builtinType | Given builtin type. |
|
inline |
This function returns builtin type.
|
inlineoverridevirtual |
This function return true/false value for identify binary type.
| true | When builtin type is binary. |
| false | When builtin type isn't binary. |
Reimplemented from erpcgen::DataType.
|
inlineoverridevirtual |
This function return "true" value for identify bool type.
| true | When builtin type is bool. |
| false | When builtin type isn't bool. |
Reimplemented from erpcgen::DataType.
|
inlineoverridevirtual |
This function return "true" value for identify float type.
| true | When builtin type is float. |
| false | When builtin type isn't float. |
Reimplemented from erpcgen::DataType.
|
inlineoverridevirtual |
This function return "true" value for identify int type.
| true | When builtin type is int. |
| false | When builtin type isn't int. |
Reimplemented from erpcgen::DataType.
|
inlineoverridevirtual |
This function return "true" value for identify scalar type.
| true | When builtin type is integer, float or boolean. |
| false | When builtin type isn't integer, float or boolean. |
Reimplemented from erpcgen::DataType.
|
inlineoverridevirtual |
This function return true/false value for identify string type.
| true | When builtin type is string or ustring. |
| false | When builtin type isn't string or ustring. |
Reimplemented from erpcgen::DataType.
|
inlineoverridevirtual |
This function return true/false value for identify ustring type.
| true | When builtin type is ustring. |
| false | When builtin type isn't ustring. |
Reimplemented from erpcgen::DataType.
|
protected |
Builtin type of current object.