Overview
========
This example works as two USB CDC ACM devices. It will appear as two USB serial devices on PC.


Toolchain supported
===================
- IAR embedded Workbench  9.40.1
- Keil MDK  5.38.1
- GCC ARM Embedded  12.2
- MCUXpresso  11.8.0

Hardware requirements
=====================
- Two Micro USB cables
- Target Board
- Personal Computer(PC)

Board settings
==============
Set USB port J3 to device mode by opening jumper JP2.

Prepare the Demo
================
1.  Connect a USB Micro cable between the host PC and the Debug Link USB port (J1) on the target board.
2.  Connect a USB Micro cable between the host PC and the on-board USB full speed port (J3).
3.  Open a serial terminal on PC with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - 1 stop bit
    - No flow control
4.  Download the program to the target board.
5.  Press the on-board RESET button to start the demo.
6.  Open two serial terminals with the following settings for two new USB serial devices.
    - 115200 baud rate
    - 8 data bits
    - No parity
    - 1 stop bit
    - No flow control

Running the demo
================
When the demo is running, the serial port of the Debug Link will output:

Start USBX device composite example...

Then, connect a USB cable between PC and the USB device port of the board.
Two USB serial devices will appear in the Device Manager of Windows.
And the serial port will output:

CDC ACM1 device activate
CDC ACM2 device activate

ACM1 device serial terminal, press any key, and it will display a string, for example:

fabcdef
gabcdef
3abcdef

ACM2 device serial terminal, press any key, and it will display a string, for example:

f123456
g123456
3123456