Overview
========
This example illustrates USBX Host Mass Storage.


Toolchain supported
===================
- IAR embedded Workbench  9.40.1
- Keil MDK  5.38.1
- GCC ARM Embedded  12.2
- MCUXpresso  11.8.0

Hardware requirements
=====================
- Two Micro USB cables
- One USB A Female to Micro B Male cable
- A U-disk device
- Target Board
- Personal Computer(PC)

Board settings
==============
Short the JP2 jumper.

Prepare the Demo
================
1.  Connect the USB A Female to Micro B Male cable between the U-disk device and
    the on-board USB full speed port (J3).
2.  Connect a USB Micro cable between the host PC and the Debug Link USB port (J1) on the target board.
3.  Connect a USB Micro cable between the PC and the on-board USB power port (J2).
4.  Open a serial terminal on the PC with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
5.  Compile the demo.
6.  Download the program to the target board.
7.  Press the on-board RESET button to start the demo.

Running the demo
================
After writing the program to the flash of the target board,
press the reset button on your board to start the demo.
The serial port will output:

USBX host mass storage example

Then, connect a U-disk to the USB device port of the board.
The example will display the vendor ID and the product ID of
the attached USB device, then scan the disk and dump the file
name to the serial port.

For example:

USB device: vid=0x2ce3, pid=0x6487
Find Dir: DIR_1
Find Dir: DIR_2
Find File: 1234.text
Find File: test.text