Overview
========
The CTimer Example project is to demonstrate usage of the KSDK ctimer driver.
In this example, the match feature of the CTimer is used to toggle the output level.

Toolchain supported
===================
- IAR embedded Workbench  9.40.1
- Keil MDK  5.38.1
- GCC ARM Embedded  12.2
- MCUXpresso  11.8.0

Hardware requirements
=====================
- Micro USB cable
- LPCXpresso55S36 board
- Personal Computer

Board settings
==============

Prepare the Demo
================
1.  Connect a micro USB cable between the host PC and the LPC-Link USB port (J1) on the target board.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo
================
The log below shows example output of the CTimer driver simple match demo in the terminal window:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
CTimer match example to toggle the output on a match
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

You can see the red led blinking on board.