Overview
========
The SCTimer project is a simple demonstration program of the SDK SCTimer's driver capabiltiy to generate PWM signals.
The SCTimer project enables a 32-bit counter to output two center-aligned PWM signals with parameters set to 24kHz frequency.
The duty cycles of the two PWM signals are 50% and 20%, respectively.

Toolchain supported
===================
- IAR embedded Workbench  9.40.1
- Keil MDK  5.38.1
- GCC ARM Embedded  12.2
- MCUXpresso  11.8.0

Hardware requirements
=====================
- Micro USB cable
- LPCXpresso55S36 board
- Personal Computer

# Board settings

```
Output signal		Board location
SCT0_OUT0    		J10-5 (P1_4)
SCT0_OUT4    		J10-13(P1_17)
```

# Prepare the Demo

1.  Connect a micro USB cable between the host PC and the LPC-Link USB port (J1) on the target board.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo
================
The log below shows example output of the SCTimer driver simple PWM demo in the terminal window:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
SCTimer example to output 2 center-aligned PWM signals

Probe the signal using an oscilloscope
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

You'll see center-aligned PWM signals on J10-5 and J10-13 using an oscilloscope.