Overview
========
The Trusted Firmware M (TF-M) demo application provides a sanity check for the TF-M core and RoT services.
It can be used as a template for a new application which requires functionality of the TF-M Secure Services.

NOTE: The TF-M main() functions have a non-standard location:
       - Secure main() is in the tf-m\secure_fw\spm\cmsis_psa\main.c file.
       - Non-Secure main() is in the tf-m-tests\app\main_ns.c file.

Toolchain supported
===================
- GCC ARM Embedded  12.2
- Keil MDK  5.38.1
- IAR embedded Workbench  9.40.1
- MCUXpresso  11.8.0

Hardware requirements
=====================
- Micro USB cable
- LPCXpresso55S36 board
- Personal Computer

Board settings
==============
No special settings are required.

Prepare the Demo
================
1.  Connect a micro USB cable between the PC host and the CMSIS DAP USB port on the board
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Use secure project to download the program to target board. Please refer to "TrustZone application debugging" below for details.
4.  Launch the debugger in your IDE to begin running the demo.

Running the demo
================
The log below shows the output of the TFM demo in the terminal window:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
[INF] Beginning TF-M provisioning
[WRN] TFM_DUMMY_PROVISIONING is not suitable for production! This device is NOT SECURE
[Sec Thread] Secure image initializing!
TF-M FP mode: Hardware
Lazy stacking enabled
Booting TF-M 1.6.0
Creating an empty ITS flash layout.
Creating an empty PS flash layout.
[INF][Crypto] Initialising HW accelerator... complete.
Non-Secure system starting...
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~


TrustZone Application Development in SDK
----------------------------------------
Every TrustZone based application consists of two independent parts - secure part/project and non-secure part/project.

The secure project is stored in <application_name>\<application_name>_s directory.
The non-secure project is stored in <application_name>\<application_name>_ns directory. 

The secure projects always contains TrustZone configuration and it is executed after device RESET. The secure project usually
ends by jump to non-secure application/project.
If IDE allows the two projects in single workspace, the user can also find the project with <application_name>.
This project contains both secure and non-secure projects in one workspace (Keil MDK, IAR) and it allows to user easy transition from
one to another project.

TrustZone application compilation
--------------------------------
Please compile secure project firstly since CMSE library is needed for compilation of non-secure project.
After successful compilation of secure project, compile non-secure project.

TrustZone application debugging
-------------------------------
- Download both output file into device memory
- Start execution of secure project since secure project is going to be executed after device RESET.

If IDE (Keil MDK, IAR) allows to manage download both output files as single download, the secure project
is configured to download both secure and non-secure output files so debugging can be fully managed
from secure project.

Device header file and secure/non-secure access to the peripherals
------------------------------------------------------------------
Both secure and non-secure project uses identical device header file. The access to secure and non-secure aliases for all peripherals
is managed using compiler macro __ARM_FEATURE_CMSE.

For secure project using <PERIPH_BASE> means access through secure alias (address bit A28=1), 
using <PERIPH_BASE>_NS means access through non-secure alias(address bit A28=0)
For non-secure project using <PERIPH_BASE> means access through non-secure alias (address bit A28=0). 
The non-secure project doesn't have access to secure memory or peripherals regions so the secure access is not defined.