Overview
========
The Trusted Firmware M (TF-M) PSA Dev API test application provides verification that secure service API behaviours are implemented correctly.
The PSA Dev API tests are the basis for getting the PSA Functional API Certification.

NOTE: The TF-M main() functions have a non-standard location:
       - Secure main() is in the tf-m\secure_fw\spm\cmsis_psa\main.c file.
       - Non-Secure main() is in the tf-m-tests\app\main_ns.c file.

Toolchain supported
===================
- GCC ARM Embedded  12.2
- Keil MDK  5.38.1
- IAR embedded Workbench  9.40.1
- MCUXpresso  11.8.0

Hardware requirements
=====================
- Mini/micro USB cable
- LPCXpresso55S36 board
- Personal Computer

Board settings
==============
No special settings are required.

Prepare the Demo
================
1.  Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board
2.  Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Use secure project to download the program to target board
    For IAR environment go to project options/Debugger/Images. Open file dialog for first extra image. Select file <application_name>_ns.out and click on open button. 
    Now you have absolute path in the path box. The flash loader requires absolute path to this file.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo
================
The log below shows the output of the TFM PSA API tests in the terminal window:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
[INF] Beginning TF-M provisioning
[WRN] TFM_DUMMY_PROVISIONING is not suitable for production! This device is NOT SECURE
[Sec Thread] Secure image initializing!
TF-M FP mode: Hardware
Lazy stacking enabled
Booting TF-M 1.6.0
Creating an empty ITS flash layout.
Creating an empty PS flash layout.
[INF][Crypto] Initialising HW accelerator... complete.
Non-Secure system starting...

***** PSA Architecture Test Suite - Version 1.4 *****

Running.. Crypto Suite
******************************************

TEST: 201 | DESCRIPTION: Testing crypto key management APIs | UT:  psa_crypto_init
[Info] Executing tests from non-secure
[Check 1] Test calling crypto functions before psa_crypto_init
[Check 2] Test psa_crypto_init
[Check 3] Test multiple psa_crypto_init

TEST RESULT: PASSED

******************************************

TEST: 202 | DESCRIPTION: Testing crypto key management APIs | UT: psa_import_key
[Info] Executing tests from non-secure
[Check 1] Test psa_import_key with EC Public key

TEST RESULT: PASSED

******************************************

TEST: 203 | DESCRIPTION: Testing crypto key management APIs | UT: psa_export_key
[Info] Executing tests from non-secure
[Check 1] Test psa_export_key with EC Public key

TEST RESULT: PASSED

******************************************

TEST: 204 | DESCRIPTION: Testing crypto key management APIs | UT: psa_export_public_key
[Info] Executing tests from non-secure
[Check 1] Test psa_export_public_key with EC Public key

TEST RESULT: PASSED

******************************************

TEST: 205 | DESCRIPTION: Testing crypto key management APIs | UT: psa_destroy_key
[Info] Executing tests from non-secure
[Check 1] Test psa_destroy_key with EC Public key

TEST RESULT: PASSED

******************************************

TEST: 208 | DESCRIPTION: Testing crypto key derivation APIs | UT: psa_key_derivation_setup
[Info] Executing tests from non-secure
[Check 1] Test psa_key_derivation_setup - ECDH + HKDF-SHA-256
[Check 2] Test psa_key_derivation_setup - ECDH, unknown KDF
[Check 3] Test psa_key_derivation_setup - bad key derivation algorithm
[Check 4] Test psa_key_derivation_setup - Invalid Algorithm

TEST RESULT: PASSED

******************************************

TEST: 210 | DESCRIPTION: Testing crypto key attributes APIs | UT: psa_key_attributes_set_get
[Info] Executing tests from non-secure
[Check 1] Test psa_key_attributes_set_get key attributes

TEST RESULT: PASSED

******************************************

TEST: 211 | DESCRIPTION: Testing crypto hash functions APIs | UT: psa_hash_setup
[Info] Executing tests from non-secure
[Check 1] Test psa_hash_setup with SHA256 algorithm
[Check 2] Test psa_hash_setup with Invalid hash algorithm
[Check 3] Test psa_hash_setup with Invalid algorithm
[Check 4] Test psa_hash_setup with CTR algorithm

TEST RESULT: PASSED

******************************************

TEST: 212 | DESCRIPTION: Testing crypto hash functions APIs | UT: psa_hash_update
[Info] Executing tests from non-secure
[Check 1] Test psa_hash_update with SHA256 algorithm
[Check 2] Test psa_hash_update without hash setup
[Check 3] Test psa_hash_update with completed opertaion handle

TEST RESULT: PASSED

******************************************

TEST: 213 | DESCRIPTION: Testing crypto hash functions APIs | UT: psa_hash_verify
[Info] Executing tests from non-secure
[Check 1] Test psa_hash_verify with SHA256 algorithm
[Check 2] Test psa_hash_verify with incorrect expected hash
[Check 3] Test psa_hash_verify with incorrect hash length
[Check 4] test psa_hash_verify with inactive & invalid operation handle

TEST RESULT: PASSED

******************************************

TEST: 214 | DESCRIPTION: Testing crypto hash functions APIs | UT: psa_hash_finish
[Info] Executing tests from non-secure
[Check 1] Test psa_hash_finish with SHA256 algorithm
[Check 2] Test psa_hash_finish with invalid hash buffer size
[Check 3] test psa_hash_finish with inactive operation handle

TEST RESULT: PASSED

******************************************

TEST: 215 | DESCRIPTION: Testing crypto hash functions APIs | UT: psa_hash_abort
[Info] Executing tests from non-secure
[Check 1] Test psa_hash_abort with SHA256 algorithm
[Check 2] Test psa_hash_finish after calling psa_hash_abort

TEST RESULT: PASSED

******************************************

TEST: 216 | DESCRIPTION: Testing crypto generator functions APIs | UT: psa_generate_key
[Info] Executing tests from non-secure
[Check 1] Test psa_generate_key with invalid key type
[Check 2] Test psa_generate_key with invalid usage flags

TEST RESULT: PASSED

******************************************

TEST: 217 | DESCRIPTION: Testing crypto generation APIs | UT: psa_generate_random
[Info] Executing tests from non-secure
[Check 1] Test psa_generate_random to get 0 Byte data
[Check 2] Test psa_generate_random to get 16 Byte data
[Check 3] Test psa_generate_random to get 24 Byte data
[Check 4] Test psa_generate_random to get 32 Byte data
[Check 5] Test psa_generate_random to get 64 Byte data
[Check 6] Test psa_generate_random to get 128 Byte data
[Check 7] Test psa_generate_random to get 256 Byte data
[Check 8] Test psa_generate_random to get 512 Byte data
[Check 9] Test psa_generate_random to get 1000 Byte data

TEST RESULT: PASSED

******************************************

TEST: 218 | DESCRIPTION: Testing crypto key derivation APIs | UT: psa_key_derivation_input_key
[Info] Executing tests from non-secure
[Check 1] Test psa_key_derivation_input_key 16 Byte Key
[Check 2] Test psa_key_derivation_input_key with invalid usage
[Check 3] Test psa_key_derivation_input_key with step as label
[Check 4] Test psa_key_derivation_input_key with step as info
[Check 5] Test psa_key_derivation_input_key with step as seed
[Check 6] Test psa_key_derivation_input_key with step as salt
[Check 7] Test psa_key_derivation_input_key with key type as AES(not derive)
[Check 8] Test psa_key_derivation_input_key incorrect key algorithm
[Check 9] Test psa_key_derivation_input_key with zero as step
[Check 10] Test psa_cipher_decrypt_setup - Invalid key handle
[Check 11] Test psa_cipher_decrypt_setup - Zero as key handle

TEST RESULT: PASSED

******************************************

TEST: 219 | DESCRIPTION: Testing crypto key derivation APIs | UT: psa_key_derivation_key_agreement
[Info] Executing tests from non-secure
[Check 1] Test psa_key_derivation_key_agreement - KDF not a key agreement alg

TEST RESULT: SKIPPED (Skip Code=0x2d)

******************************************

TEST: 222 | DESCRIPTION: Testing crypto key derivation APIs | UT: psa_key_derivation_abort
[Info] Executing tests from non-secure
[Check 1] Test psa_key_derivation_abort

TEST RESULT: PASSED

******************************************

TEST: 223 | DESCRIPTION: Testing crypto key derivation APIs | UT: psa_key_derivation_set_get_capacity
[Info] Executing tests from non-secure
[Check 1] Test psa_key_derivation_set_get_capacity - < operation's capacity
[Check 2] Test psa_key_derivation_set_get_capacity - = operation's capacity
[Check 3] Test psa_key_derivation_set_get_capacity - > operation's capacity
[Check 4] Test psa_key_derivation_set_get_capacity - unchanged capacity

TEST RESULT: PASSED

******************************************

TEST: 224 | DESCRIPTION: Testing crypto AEAD APIs | UT: psa_aead_encrypt
[Info] Executing tests from non-secure
[Check 1] Test psa_aead_encrypt - CCM - AES - 13B nonce & 8B add data
[Check 2] Test psa_aead_encrypt - CCM - AES - 13B nonce & 32B add data
[Check 3] Test psa_aead_encrypt - CCM - AES - 24 bytes Tag length = 4
[Check 4] Test psa_aead_encrypt - CCM - AES - Zero additional data
[Check 5] Test psa_aead_encrypt - CCM - AES - Zero plaintext
[Check 6] Test psa_aead_encrypt - Unsupported algorithm
[Check 7] Test psa_aead_encrypt - Invalid usage flag
[Check 8] Test psa_aead_encrypt - Invalid ciphertext_size
[Check 9] Test psa_aead_encrypt - Invalid nonce
[Check 10] Test psa_aead_encrypt - Invalid tag length 0

TEST RESULT: PASSED

******************************************

TEST: 225 | DESCRIPTION: Testing crypto AEAD APIs | UT: psa_aead_decrypt
[Info] Executing tests from non-secure
[Check 1] Test psa_aead_decrypt - CCM - AES - 13B nonce & 8B add data
[Check 2] Test psa_aead_decrypt - CCM - AES - 13B nonce & 32B add data
[Check 3] Test psa_aead_decrypt - CCM - AES - 24 bytes Tag length = 4
[Check 4] Test psa_aead_decrypt - CCM - AES - Zero additional data
[Check 5] Test psa_aead_decrypt - CCM - AES - Zero plaintext
[Check 6] Test psa_aead_decrypt - Unsupported algorithm
[Check 7] Test psa_aead_decrypt - Invalid usage flag
[Check 8] Test psa_aead_decrypt - Invalid plaintext_size
[Check 9] Test psa_aead_decrypt - Invalid nonce
[Check 10] Test psa_aead_decrypt - Invalid cihpertext
[Check 11] Test psa_aead_decrypt - Invalid cihpertext_size
[Check 12] Test psa_aead_decrypt - Invalid tag length 0

TEST RESULT: PASSED

******************************************

TEST: 231 | DESCRIPTION: Testing crypto MAC APIs | UT: psa_mac_abort
[Info] Executing tests from non-secure
[Check 1] Test psa_mac_abort - HMAC - SHA256
[Check 2] Test psa_mac_sign_finish after calling psa_mac_abort

TEST RESULT: PASSED

******************************************

TEST: 232 | DESCRIPTION: Testing crypto symmetric cipher APIs | UT: psa_cipher_encrypt_setup
[Info] Executing tests from non-secure
[Check 1] Test psa_cipher_encrypt_setup - unknown cipher algorithm
[Check 2] Test psa_cipher_encrypt_setup - EC Public key
[Check 3] Test psa_cipher_encrypt_setup - Invalid key handle
[Check 4] Test psa_cipher_encrypt_setup - Zero as key handle

TEST RESULT: PASSED

******************************************

TEST: 233 | DESCRIPTION: Testing crypto symmetric cipher APIs | UT: psa_cipher_decrypt_setup
[Info] Executing tests from non-secure
[Check 1] Test psa_cipher_decrypt_setup - unknown cipher algorithm
[Check 2] Test psa_cipher_decrypt_setup - EC Public key
[Check 3] Test psa_cipher_decrypt_setup - Invalid key handle
[Check 4] Test psa_cipher_decrypt_setup - Zero as key handle

TEST RESULT: PASSED

******************************************

TEST: 239 | DESCRIPTION: Testing crypto asymmetric APIs | UT: psa_asymmetric_encrypt
[Info] Executing tests from non-secure
No test available for the selected crypto configuration

TEST RESULT: SKIPPED (Skip Code=0x2d)

******************************************

TEST: 240 | DESCRIPTION: Testing crypto asymmetric APIs | UT: psa_asymmetric_decrypt
[Info] Executing tests from non-secure
No test available for the selected crypto configuration

TEST RESULT: SKIPPED (Skip Code=0x2d)

******************************************

TEST: 241 | DESCRIPTION: Testing crypto asymmetric APIs | UT: psa_sign_hash
[Info] Executing tests from non-secure
[Check 1] Test psa_sign_hash - ECDSA SECP256R1 SHA-256
[Check 2] Test psa_sign_hash - Invalid key handle
[Check 3] Test psa_sign_hash - Zero as key handle

TEST RESULT: PASSED

******************************************

TEST: 242 | DESCRIPTION: Testing crypto asymmetric APIs | UT: psa_verify_hash
[Info] Executing tests from non-secure
[Check 1] Test psa_verify_hash - ECDSA KEY_PAIR SECP256R1 SHA-256
[Check 2] Test psa_verify_hash - EC public key
[Check 3] Test psa_verify_hash - Invalid key handle
[Check 4] Test psa_verify_hash - Zero as key handle

TEST RESULT: PASSED

******************************************

TEST: 243 | DESCRIPTION: Testing crypto key derivation APIs | UT: psa_raw_key_agreement
[Info] Executing tests from non-secure
[Check 1] Test psa_raw_key_agreement - Not a key agreement alg

TEST RESULT: PASSED

******************************************

TEST: 244 | DESCRIPTION: Testing crypto key management APIs | UT: psa_copy_key
[Info] Executing tests from non-secure
[Check 1] Test psa_copy_key - EC Public key

TEST RESULT: PASSED

******************************************

TEST: 245 | DESCRIPTION: Testing crypto hash functions APIs | UT: psa_hash_clone
[Info] Executing tests from non-secure
[Check 1] Test psa_hash_clone - SHA256 algorithm
[Check 2] Test psa_hash_clone - from an inactive source operation
[Check 3] Test psa_hash_clone - on an active target operation

TEST RESULT: PASSED

******************************************

************ Crypto Suite Report **********
TOTAL TESTS     : 30
TOTAL PASSED    : 27
TOTAL SIM ERROR : 0
TOTAL FAILED    : 0
TOTAL SKIPPED   : 3
******************************************

Running.. Attestation Suite
******************************************

TEST: 601 | DESCRIPTION: Testing attestation initial attestation APIs | UT: psa_initial_attestation
[Info] Executing tests from non-secure
[Check 1] Test psa_initial_attestation_get_token with Challenge 32
[Check 2] Test psa_initial_attestation_get_token with Challenge 48
[Check 3] Test psa_initial_attestation_get_token with Challenge 64
[Check 4] Test psa_initial_attestation_get_token with zero challenge size
[Check 5] Test psa_initial_attestation_get_token with small challenge size
[Check 6] Test psa_initial_attestation_get_token with invalid challenge size
[Check 7] Test psa_initial_attestation_get_token with large challenge size
[Check 8] Test psa_initial_attestation_get_token with zero as token size
[Check 9] Test psa_initial_attestation_get_token with small token size
[Check 10] Test psa_initial_attestation_get_token_size with Challenge 32
[Check 11] Test psa_initial_attestation_get_token_size with Challenge 48
[Check 12] Test psa_initial_attestation_get_token_size with Challenge 64
[Check 13] Test psa_initial_attestation_get_token_size with zero challenge size
[Check 14] Test psa_initial_attestation_get_token_size with small challenge size
[Check 15] Test psa_initial_attestation_get_token_size with invalid challenge size
[Check 16] Test psa_initial_attestation_get_token_size with large challenge size

TEST RESULT: PASSED

******************************************

************ Attestation Suite Report **********
TOTAL TESTS     : 1
TOTAL PASSED    : 1
TOTAL SIM ERROR : 0
TOTAL FAILED    : 0
TOTAL SKIPPED   : 0
******************************************

Running.. Storage Suite
******************************************

TEST: 401 | DESCRIPTION: UID not found check | UT: ITS
[Info] Executing tests from non-secure

[Info] Executing ITS tests
[Check 1] Call get API for UID 6 which is not set
[Check 2] Call get_info API for UID 6 which is not set
[Check 3] Call remove API for UID 6 which is not set
[Check 4] Call get API for UID 6 which is removed
[Check 5] Call get_info API for UID 6 which is removed
[Check 6] Call remove API for UID 6 which is removed
Set storage for UID 6
[Check 7] Call get API for different UID 5
[Check 8] Call get_info API for different UID 5
[Check 9] Call remove API for different UID 5

[Info] Executing PS tests
[Check 1] Call get API for UID 6 which is not set
[Check 2] Call get_info API for UID 6 which is not set
[Check 3] Call remove API for UID 6 which is not set
[Check 4] Call get API for UID 6 which is removed
[Check 5] Call get_info API for UID 6 which is removed
[Check 6] Call remove API for UID 6 which is removed
Set storage for UID 6
[Check 7] Call get API for different UID 5
[Check 8] Call get_info API for different UID 5
[Check 9] Call remove API for different UID 5

TEST RESULT: PASSED

******************************************

TEST: 402 | DESCRIPTION: Write once error check | UT: ITS
[Info] Executing tests from non-secure

[Info] Executing ITS tests
[Check 1] Update the flag of UID 1 with WRITE_ONCE flag
[Check 2] Try to remove the UID 1 having WRITE_ONCE flag
[Check 3] Create a new UID 2 with WRITE_ONCE flag
[Check 4] Try to remove the UID 2 having WRITE_ONCE flag
[Check 5] Try to change the length of write_once UID 2
[Check 6] Check UID removal still fails
[Check 7] Try to change the WRITE_ONCE flag to None for UID 2
[Check 8] Check UID removal still fails

[Info] Executing PS tests
[Check 1] Update the flag of UID 1 with WRITE_ONCE flag
[Check 2] Try to remove the UID 1 having WRITE_ONCE flag
[Check 3] Create a new UID 2 with WRITE_ONCE flag
[Check 4] Try to remove the UID 2 having WRITE_ONCE flag
[Check 5] Try to change the length of write_once UID 2
[Check 6] Check UID removal still fails
[Check 7] Try to change the WRITE_ONCE flag to None for UID 2
[Check 8] Check UID removal still fails

TEST RESULT: PASSED

******************************************

TEST: 403 | DESCRIPTION: Insufficient space check | UT: ITS
[Info] Executing tests from non-secure

[Info] Executing ITS tests
[Check 1] Overload storage space
UID 7 set failed due to insufficient space
Remove all registered UIDs
[Check 2] Overload storage again to verify all previous UID removed
UID 7 set failed due to insufficient space
Remove all registered UIDs

[Info] Executing PS tests
[Check 1] Overload storage space
UID 6 set failed due to insufficient space
Remove all registered UIDs
[Check 2] Overload storage again to verify all previous UID removed
UID 6 set failed due to insufficient space
Remove all registered UIDs

TEST RESULT: PASSED

******************************************

TEST: 404 | DESCRIPTION: Data Consistency check | UT: ITS
[Info] Executing tests from non-secure

[Info] Executing ITS tests
[Check 1] Call set API with reduced length - TEST_BUFF_SIZE/2
[Check 2] Call get API with default length - TEST_BUFF_SIZE

[Info] Executing PS tests
[Check 1] Call set API with reduced length - TEST_BUFF_SIZE/2
[Check 2] Call get API with default length - TEST_BUFF_SIZE

TEST RESULT: PASSED

******************************************

TEST: 405 | DESCRIPTION: Success scenarios check | UT: ITS
[Info] Executing tests from non-secure

[Info] Executing ITS tests
[Check 1] Set UID with data length zero and call storage APIs
[Check 2] Resetting the length check

[Info] Executing PS tests
[Check 1] Set UID with data length zero and call storage APIs
[Check 2] Resetting the length check

TEST RESULT: PASSED

******************************************

TEST: 406 | DESCRIPTION: Check for storage create flags | UT: ITS
[Info] Executing tests from non-secure

[Info] Executing ITS tests
[Check 1] Call set API with flag - PSA_STORAGE_FLAG_NONE
[Check 2] Call set API with flag - PSA_STORAGE_FLAG_NO_CONFIDENTIALITY
[Check 3] Call set API with flag - PSA_STORAGE_FLAG_NO_REPLAY_PROTECTION

[Info] Executing PS tests
[Check 1] Call set API with flag - PSA_STORAGE_FLAG_NONE
[Check 2] Call set API with flag - PSA_STORAGE_FLAG_NO_CONFIDENTIALITY
[Check 3] Call set API with flag - PSA_STORAGE_FLAG_NO_REPLAY_PROTECTION

TEST RESULT: PASSED

******************************************

TEST: 407 | DESCRIPTION: Incorrect Size check | UT: ITS
[Info] Executing tests from non-secure

[Info] Executing ITS tests
Create a valid Storage - TEST_BUFF_SIZE/2
Increase the length of storage - TEST_BUFF_SIZE
[Check 1] Call get API with old length - TEST_BUFF_SIZE/2
[Check 2] Call get API with old length - TEST_BUFF_SIZE/4
Decrease the length of storage - TEST_BUFF_SIZE/4
[Check 3] Call get API with old length - TEST_BUFF_SIZE/2
[Check 4] Call get API with old length - TEST_BUFF_SIZE
[Check 5] Call get API with valid length - TEST_BUFF_SIZE/4

[Info] Executing PS tests
Create a valid Storage - TEST_BUFF_SIZE/2
Increase the length of storage - TEST_BUFF_SIZE
[Check 1] Call get API with old length - TEST_BUFF_SIZE/2
[Check 2] Call get API with old length - TEST_BUFF_SIZE/4
Decrease the length of storage - TEST_BUFF_SIZE/4
[Check 3] Call get API with old length - TEST_BUFF_SIZE/2
[Check 4] Call get API with old length - TEST_BUFF_SIZE
[Check 5] Call get API with valid length - TEST_BUFF_SIZE/4

TEST RESULT: PASSED

******************************************

TEST: 408 | DESCRIPTION: Invalid offset check | UT: ITS
[Info] Executing tests from non-secure

[Info] Executing ITS tests
[Check 1] Try to access data with varying valid offset
[Check 2] Try to access data with varying invalid offset

[Info] Executing PS tests
[Check 1] Try to access data with varying valid offset
[Check 2] Try to access data with varying invalid offset

TEST RESULT: PASSED

******************************************

TEST: 409 | DESCRIPTION: Invalid Arguments check | UT: ITS
[Info] Executing tests from non-secure

[Info] Executing ITS tests
[Check 1] Call set API with NULL pointer and data length 0
[Check 2] Call get API with NULL read buffer and data length 0
[Check 3] Remove the UID
[Check 4] Call get_info API to verify UID removed
[Check 5] Create UID with zero data_len and valid write buffer
[Check 8] Call get API with NULL read buffer and data length 0
[Check 9] Increase the length

[Info] Executing PS tests
[Check 1] Call set API with NULL pointer and data length 0
[Check 2] Call get API with NULL read buffer and data length 0
[Check 3] Remove the UID
[Check 4] Call get_info API to verify UID removed
[Check 5] Create UID with zero data_len and valid write buffer
[Check 8] Call get API with NULL read buffer and data length 0
[Check 9] Increase the length

TEST RESULT: PASSED

******************************************

TEST: 410 | DESCRIPTION: UID value zero check | UT: ITS
[Info] Executing tests from non-secure

[Info] Executing ITS tests
[Check 1] Creating storage with UID 0 should fail
[Check 2] Get_info for UID 0 should fail
[Check 3] Removing storage with UID 0 should fail

[Info] Executing PS tests
[Check 1] Creating storage with UID 0 should fail
[Check 2] Get_info for UID 0 should fail
[Check 3] Removing storage with UID 0 should fail

TEST RESULT: PASSED

******************************************

TEST: 411 | DESCRIPTION: Optional APIs: UID not found check | UT: ITS
[Info] Executing tests from non-secure

[Info] Executing PS tests
Test Case skipped as Optional PS APIs are not supported.

TEST RESULT: SKIPPED (Skip Code=0x2b)

******************************************

TEST: 412 | DESCRIPTION: Optional APIs: Invalid arguments and offset invalid | UT: ITS
[Info] Executing tests from non-secure

[Info] Executing PS tests
Test Case skipped as Optional PS APIs are not supported.

TEST RESULT: SKIPPED (Skip Code=0x2b)

******************************************

TEST: 413 | DESCRIPTION: Set_Extended and Create api : Success | UT: ITS
[Info] Executing tests from non-secure

[Info] Executing PS tests
Test Case skipped as Optional PS APIs are not supported.

TEST RESULT: SKIPPED (Skip Code=0x2b)

******************************************

TEST: 414 | DESCRIPTION: Optional APIs not supported check | UT: ITS
[Info] Executing tests from non-secure

[Info] Executing PS tests
Optional PS APIs are not supported.
[Check 1] Call to create API should fail as API not supported
[Check 2] Create valid storage with set API
[Check 3] Call to set_extended API call should fail
[Check 4] Verify data is unchanged

TEST RESULT: PASSED

******************************************

TEST: 415 | DESCRIPTION: Create API write_once flag value check | UT: ITS
[Info] Executing tests from non-secure

[Info] Executing PS tests
Test Case skipped as Optional PS APIs are not supported.

TEST RESULT: SKIPPED (Skip Code=0x2b)

******************************************

TEST: 416 | DESCRIPTION: Storage assest capacity modification check | UT: ITS
[Info] Executing tests from non-secure

[Info] Executing PS tests
Test Case skipped as Optional PS APIs not are supported.

TEST RESULT: SKIPPED (Skip Code=0x2b)

******************************************

TEST: 417 | DESCRIPTION: Storage assest capacity modification check | UT: ITS
[Info] Executing tests from non-secure

[Info] Executing PS tests
Test Case skipped as Optional PS APIs not are supported.

TEST RESULT: SKIPPED (Skip Code=0x2b)

******************************************

************ Storage Suite Report **********
TOTAL TESTS     : 17
TOTAL PASSED    : 11
TOTAL SIM ERROR : 0
TOTAL FAILED    : 0
TOTAL SKIPPED   : 6
******************************************

Entering standby..

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~