Overview
========
The Trusted Firmware M (TF-M) certification application which is provided to a PSA Certification laboratory.

NOTE: The TF-M main() functions have a non-standard location:
       - Secure main() is in the tf-m\secure_fw\spm\cmsis_psa\main.c file.
       - Non-Secure main() is in the tf-m-tests\app\main_ns.c file.

Toolchain supported
===================
- Keil MDK  5.38.1

Hardware requirements
=====================
- Mini/micro USB cable
- LPCXpresso55S36 board
- Personal Computer

Board settings
==============
No special settings are required.

Prepare the Demo
================
1.  Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board
2.  Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Use secure project to download the program to target board
    For IAR environment go to project options/Debugger/Images. Open file dialog for first extra image. Select file <application_name>_ns.out and click on open button. 
    Now you have absolute path in the path box. The flash loader requires absolute path to this file.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo
================
The log below shows the output of the TFM PSA API tests in the terminal window:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
[WRN] This device was provisioned with dummy keys. This device is NOT SECURE
[Sec Thread] Secure image initializing!
TF-M Float ABI: Hard
Lazy stacking enabled
Booting TF-M 1.7.0
Non-Secure system starting...

***** PSA Architecture Test Suite - Version 1.4 *****

Running.. Crypto Suite
******************************************

TEST: 201 | DESCRIPTION: Testing crypto key management APIs | UT:  psa_crypto_init
[Info] Executing tests from non-secure
[Check 1] Test calling crypto functions before psa_crypto_init
[Check 2] Test psa_crypto_init
[Check 3] Test multiple psa_crypto_init

TEST RESULT: PASSED

******************************************

TEST: 202 | DESCRIPTION: Testing crypto key management APIs | UT: psa_import_key
[Info] Executing tests from non-secure
[Check 1] Test psa_import_key with EC Public key

TEST RESULT: PASSED

******************************************

TEST: 203 | DESCRIPTION: Testing crypto key management APIs | UT: psa_export_key
[Info] Executing tests from non-secure
[Check 1] Test psa_export_key with EC Public key

TEST RESULT: PASSED

******************************************

TEST: 204 | DESCRIPTION: Testing crypto key management APIs | UT: psa_export_public_key
[Info] Executing tests from non-secure
[Check 1] Test psa_export_public_key with EC Public key

TEST RESULT: PASSED

******************************************

TEST: 205 | DESCRIPTION: Testing crypto key management APIs | UT: psa_destroy_key
[Info] Executing tests from non-secure
[Check 1] Test psa_destroy_key with EC Public key

TEST RESULT: PASSED

******************************************

TEST: 206 | DESCRIPTION: Testing crypto hash functions APIs | UT: psa_hash_compute
[Info] Executing tests from non-secure
[Check 1] Test psa_hash_compute with SHA256 algorithm
[Check 2] Test psa_hash_compute with invalid algorithm

TEST RESULT: PASSED

******************************************

TEST: 207 | DESCRIPTION: Testing crypto hash functions APIs | UT: psa_hash_compare
[Info] Executing tests from non-secure
[Check 1] Test psa_hash_compare with SHA256 algorithm
[Check 2] Test psa_hash_compare with incorrect hash
[Check 3] Test psa_hash_compare with incorrect hash length
[Check 4] Test psa_hash_compare with invalid algorithm

TEST RESULT: PASSED

******************************************

TEST: 208 | DESCRIPTION: Testing crypto key derivation APIs | UT: psa_key_derivation_setup
[Info] Executing tests from non-secure
[Check 1] Test psa_key_derivation_setup - ECDH + HKDF-SHA-256
[Check 2] Test psa_key_derivation_setup - ECDH, unknown KDF
[Check 3] Test psa_key_derivation_setup - bad key derivation algorithm
[Check 4] Test psa_key_derivation_setup - Invalid Algorithm

TEST RESULT: PASSED

******************************************

TEST: 209 | DESCRIPTION: Testing crypto key derivation APIs | UT: psa_key_derivation_input_bytes
[Info] Executing tests from non-secure
[Check 1] Test psa_key_derivation_input_bytes - Step as Info
[Check 2] Test psa_key_derivation_input_bytes - Step as secret
[Check 3] Test psa_key_derivation_input_bytes - Step as salt
[Check 4] Test psa_key_derivation_input_bytes - Step as label
[Check 5] Test psa_key_derivation_input_bytes - Step as seed
[Check 6] Test psa_key_derivation_input_bytes - Invalid step

TEST RESULT: PASSED

******************************************

TEST: 210 | DESCRIPTION: Testing crypto key attributes APIs | UT: psa_key_attributes_set_get
[Info] Executing tests from non-secure
[Check 1] Test psa_key_attributes_set_get key attributes

TEST RESULT: PASSED

******************************************

TEST: 211 | DESCRIPTION: Testing crypto hash functions APIs | UT: psa_hash_setup
[Info] Executing tests from non-secure
[Check 1] Test psa_hash_setup with SHA256 algorithm
[Check 2] Test psa_hash_setup with Invalid hash algorithm
[Check 3] Test psa_hash_setup with Invalid algorithm
[Check 4] Test psa_hash_setup with CTR algorithm

TEST RESULT: PASSED

******************************************

TEST: 212 | DESCRIPTION: Testing crypto hash functions APIs | UT: psa_hash_update
[Info] Executing tests from non-secure
[Check 1] Test psa_hash_update with SHA256 algorithm
[Check 2] Test psa_hash_update without hash setup
[Check 3] Test psa_hash_update with completed opertaion handle

TEST RESULT: PASSED

******************************************

TEST: 213 | DESCRIPTION: Testing crypto hash functions APIs | UT: psa_hash_verify
[Info] Executing tests from non-secure
[Check 1] Test psa_hash_verify with SHA256 algorithm
[Check 2] Test psa_hash_verify with incorrect expected hash
[Check 3] Test psa_hash_verify with incorrect hash length
[Check 4] test psa_hash_verify with inactive & invalid operation handle

TEST RESULT: PASSED

******************************************

TEST: 214 | DESCRIPTION: Testing crypto hash functions APIs | UT: psa_hash_finish
[Info] Executing tests from non-secure
[Check 1] Test psa_hash_finish with SHA256 algorithm
[Check 2] Test psa_hash_finish with invalid hash buffer size
[Check 3] test psa_hash_finish with inactive operation handle

TEST RESULT: PASSED

******************************************

TEST: 215 | DESCRIPTION: Testing crypto hash functions APIs | UT: psa_hash_abort
[Info] Executing tests from non-secure
[Check 1] Test psa_hash_abort with SHA256 algorithm
[Check 2] Test psa_hash_finish after calling psa_hash_abort

TEST RESULT: PASSED

******************************************

TEST: 216 | DESCRIPTION: Testing crypto generator functions APIs | UT: psa_generate_key
[Info] Executing tests from non-secure
[Check 1] Test psa_generate_key with invalid key type
[Check 2] Test psa_generate_key with invalid usage flags

TEST RESULT: PASSED

******************************************

TEST: 217 | DESCRIPTION: Testing crypto generation APIs | UT: psa_generate_random
[Info] Executing tests from non-secure
[Check 1] Test psa_generate_random to get 0 Byte data
[Check 2] Test psa_generate_random to get 16 Byte data
[Check 3] Test psa_generate_random to get 24 Byte data
[Check 4] Test psa_generate_random to get 32 Byte data
[Check 5] Test psa_generate_random to get 64 Byte data
[Check 6] Test psa_generate_random to get 128 Byte data
[Check 7] Test psa_generate_random to get 256 Byte data
[Check 8] Test psa_generate_random to get 512 Byte data
[Check 9] Test psa_generate_random to get 1000 Byte data

TEST RESULT: PASSED

******************************************

TEST: 218 | DESCRIPTION: Testing crypto key derivation APIs | UT: psa_key_derivation_input_key
[Info] Executing tests from non-secure
[Check 1] Test psa_key_derivation_input_key 16 Byte Key
[Check 2] Test psa_key_derivation_input_key with invalid usage
[Check 3] Test psa_key_derivation_input_key with step as label
[Check 4] Test psa_key_derivation_input_key with step as info
[Check 5] Test psa_key_derivation_input_key with step as seed
[Check 6] Test psa_key_derivation_input_key with step as salt
[Check 7] Test psa_key_derivation_input_key with key type as AES(not derive)
[Check 8] Test psa_key_derivation_input_key incorrect key algorithm
[Check 9] Test psa_key_derivation_input_key with zero as step
[Check 10] Test psa_cipher_decrypt_setup - Invalid key handle
[Check 11] Test psa_cipher_decrypt_setup - Zero as key handle

TEST RESULT: PASSED

******************************************

TEST: 219 | DESCRIPTION: Testing crypto key derivation APIs | UT: psa_key_derivation_key_agreement
[Info] Executing tests from non-secure
[Check 1] Test psa_key_derivation_key_agreement - KDF not a key agreement alg

TEST RESULT: SKIPPED (Skip Code=0x2d)

******************************************

TEST: 220 | DESCRIPTION: Testing crypto key derivation APIs | UT: psa_key_derivation_output_bytes
[Info] Executing tests from non-secure
[Check 1] Test psa_key_derivation_output_bytes - HKDF
[Check 2] Test psa_key_derivation_output_bytes - optional salt
[Check 3] Test psa_key_derivation_output_bytes - capacity < output_length
[Check 4] Test psa_key_derivation_output_bytes - missing info
[Check 5] Test psa_key_derivation_output_bytes - missing salt/secret/info

TEST RESULT: PASSED

******************************************

TEST: 221 | DESCRIPTION: Testing crypto key derivation APIs | UT: psa_key_derivation_output_key
[Info] Executing tests from non-secure
[Check 1] Test psa_key_derivation_output_key - Key
[Check 2] Test psa_key_derivation_output_key - Info
[Check 3] Test psa_key_derivation_output_key - Salt
[Check 4] Test psa_key_derivation_output_key - Greater Capacity than available
[Check 5] Test psa_key_derivation_output_key - ECC Public key
[Check 6] Test psa_key_derivation_output_key -  ECC keypair (wrong key length)
[Check 7] Test psa_key_derivation_output_key -  RSA Public Key[Check 8] Test psa_key_derivation_output_key -  RSA keypair
[Check 9] Test psa_key_derivation_output_key - Invalid key size

TEST RESULT: PASSED

******************************************

TEST: 222 | DESCRIPTION: Testing crypto key derivation APIs | UT: psa_key_derivation_abort
[Info] Executing tests from non-secure
[Check 1] Test psa_key_derivation_abort

TEST RESULT: PASSED

******************************************

TEST: 223 | DESCRIPTION: Testing crypto key derivation APIs | UT: psa_key_derivation_set_get_capacity
[Info] Executing tests from non-secure
[Check 1] Test psa_key_derivation_set_get_capacity - < operation's capacity
[Check 2] Test psa_key_derivation_set_get_capacity - = operation's capacity
[Check 3] Test psa_key_derivation_set_get_capacity - > operation's capacity
[Check 4] Test psa_key_derivation_set_get_capacity - unchanged capacity

TEST RESULT: PASSED

******************************************

TEST: 224 | DESCRIPTION: Testing crypto AEAD APIs | UT: psa_aead_encrypt
[Info] Executing tests from non-secure
[Check 1] Test psa_aead_encrypt - CCM - AES - 13B nonce & 8B add data
[Check 2] Test psa_aead_encrypt - CCM - AES - 13B nonce & 32B add data
[Check 3] Test psa_aead_encrypt - CCM - AES - 24 bytes Tag length = 4
[Check 4] Test psa_aead_encrypt - CCM - AES - Zero additional data
[Check 5] Test psa_aead_encrypt - CCM - AES - Zero plaintext
[Check 6] Test psa_aead_encrypt - Unsupported algorithm
[Check 7] Test psa_aead_encrypt - Invalid usage flag
[Check 8] Test psa_aead_encrypt - Invalid ciphertext_size
[Check 9] Test psa_aead_encrypt - Invalid nonce
[Check 10] Test psa_aead_encrypt - Invalid tag length 0

TEST RESULT: PASSED

******************************************

TEST: 225 | DESCRIPTION: Testing crypto AEAD APIs | UT: psa_aead_decrypt
[Info] Executing tests from non-secure
[Check 1] Test psa_aead_decrypt - CCM - AES - 13B nonce & 8B add data
[Check 2] Test psa_aead_decrypt - CCM - AES - 13B nonce & 32B add data
[Check 3] Test psa_aead_decrypt - CCM - AES - 24 bytes Tag length = 4
[Check 4] Test psa_aead_decrypt - CCM - AES - Zero additional data
[Check 5] Test psa_aead_decrypt - CCM - AES - Zero plaintext
[Check 6] Test psa_aead_decrypt - Unsupported algorithm
[Check 7] Test psa_aead_decrypt - Invalid usage flag
[Check 8] Test psa_aead_decrypt - Invalid plaintext_size
[Check 9] Test psa_aead_decrypt - Invalid nonce
[Check 10] Test psa_aead_decrypt - Invalid cihpertext
[Check 11] Test psa_aead_decrypt - Invalid cihpertext_size
[Check 12] Test psa_aead_decrypt - Invalid tag length 0

TEST RESULT: PASSED

******************************************

TEST: 226 | DESCRIPTION: Testing crypto MAC APIs | UT: psa_mac_sign_setup
[Info] Executing tests from non-secure
[Check 1] Test psa_mac_sign_setup - HMAC - SHA256
[Check 2] Test psa_mac_sign_setup - Invalid usage flag
[Check 3] Test psa_mac_sign_setup - Invalid key type
[Check 4] Test psa_mac_sign_setup - Truncated MAC too large
[Check 5] Test psa_mac_sign_setup - Truncated MAC too small
[Check 6] Test psa_mac_sign_setup - Unknown MAC algorithm
[Check 7] Test psa_mac_sign_setup invalid key handle
[Check 8] Test psa_mac_sign_setup zero as key handle

TEST RESULT: PASSED

******************************************

TEST: 227 | DESCRIPTION: Testing crypto MAC APIs | UT: psa_mac_update
[Info] Executing tests from non-secure
[Check 1] Test psa_mac_update - HMAC - SHA256 - 64 Byte

TEST RESULT: PASSED

******************************************

TEST: 228 | DESCRIPTION: Testing crypto MAC APIs | UT: psa_mac_sign_finish
[Info] Executing tests from non-secure
[Check 1] Test psa_mac_sign_finish  - HMAC - SHA256

TEST RESULT: PASSED

******************************************

TEST: 229 | DESCRIPTION: Testing crypto MAC APIs | UT: psa_mac_verify_setup
[Info] Executing tests from non-secure
[Check 1] Test psa_mac_verify_setup - HMAC - SHA256
[Check 2] Test psa_mac_verify_setup - Invalid usage flag
[Check 3] Test psa_mac_verify_setup - Invalid key type
[Check 4] Test psa_mac_verify_setup - Truncated MAC too large
[Check 5] Test psa_mac_verify_setup - Truncated MAC too small
[Check 6] Test psa_mac_verify_setup - Unknown MAC algorithm
[Check 7] Test psa_mac_verify_setup invalid key handle
[Check 8] Test psa_mac_verify_setup zero as key handle

TEST RESULT: PASSED

******************************************

TEST: 230 | DESCRIPTION: Testing crypto MAC APIs | UT: psa_mac_verify_finish
[Info] Executing tests from non-secure
[Check 1] Test psa_mac_verify_finish - HMAC - SHA256

TEST RESULT: PASSED

******************************************

TEST: 231 | DESCRIPTION: Testing crypto MAC APIs | UT: psa_mac_abort
[Info] Executing tests from non-secure
[Check 1] Test psa_mac_abort - HMAC - SHA256
[Check 2] Test psa_mac_sign_finish after calling psa_mac_abort

TEST RESULT: PASSED

******************************************

TEST: 232 | DESCRIPTION: Testing crypto symmetric cipher APIs | UT: psa_cipher_encrypt_setup
[Info] Executing tests from non-secure
[Check 1] Test psa_cipher_encrypt_setup - unknown cipher algorithm
[Check 2] Test psa_cipher_encrypt_setup - EC Public key
[Check 3] Test psa_cipher_encrypt_setup - Invalid key handle
[Check 4] Test psa_cipher_encrypt_setup - Zero as key handle

TEST RESULT: PASSED

******************************************

TEST: 233 | DESCRIPTION: Testing crypto symmetric cipher APIs | UT: psa_cipher_decrypt_setup
[Info] Executing tests from non-secure
[Check 1] Test psa_cipher_decrypt_setup - unknown cipher algorithm
[Check 2] Test psa_cipher_decrypt_setup - EC Public key
[Check 3] Test psa_cipher_decrypt_setup - Invalid key handle
[Check 4] Test psa_cipher_decrypt_setup - Zero as key handle

TEST RESULT: PASSED

******************************************

TEST: 234 | DESCRIPTION: Testing crypto symmetric cipher APIs | UT: psa_cipher_generate_iv
[Info] Executing tests from non-secure
No test available for the selected crypto configuration

TEST RESULT: SKIPPED (Skip Code=0x2d)

******************************************

TEST: 235 | DESCRIPTION: Testing crypto symmetric cipher APIs | UT: psa_cipher_set_iv
[Info] Executing tests from non-secure
No test available for the selected crypto configuration

TEST RESULT: SKIPPED (Skip Code=0x2d)

******************************************

TEST: 236 | DESCRIPTION: Testing crypto symmetric cipher APIs | UT: psa_cipher_update
[Info] Executing tests from non-secure
No test available for the selected crypto configuration

TEST RESULT: SKIPPED (Skip Code=0x2d)

******************************************

TEST: 237 | DESCRIPTION: Testing crypto symmetric cipher APIs | UT: psa_cipher_finish
[Info] Executing tests from non-secure
No test available for the selected crypto configuration

TEST RESULT: SKIPPED (Skip Code=0x2d)

******************************************

TEST: 238 | DESCRIPTION: Testing crypto symmetric cipher APIs | UT: psa_cipher_abort
[Info] Executing tests from non-secure
No test available for the selected crypto configuration

TEST RESULT: SKIPPED (Skip Code=0x2d)

******************************************

TEST: 239 | DESCRIPTION: Testing crypto asymmetric APIs | UT: psa_asymmetric_encrypt
[Info] Executing tests from non-secure
No test available for the selected crypto configuration

TEST RESULT: SKIPPED (Skip Code=0x2d)

******************************************

TEST: 240 | DESCRIPTION: Testing crypto asymmetric APIs | UT: psa_asymmetric_decrypt
[Info] Executing tests from non-secure
No test available for the selected crypto configuration

TEST RESULT: SKIPPED (Skip Code=0x2d)

******************************************

TEST: 241 | DESCRIPTION: Testing crypto asymmetric APIs | UT: psa_sign_hash
[Info] Executing tests from non-secure
[Check 1] Test psa_sign_hash - ECDSA SECP256R1 SHA-256
[Check 2] Test psa_sign_hash - Invalid key handle
[Check 3] Test psa_sign_hash - Zero as key handle

TEST RESULT: PASSED

******************************************

TEST: 242 | DESCRIPTION: Testing crypto asymmetric APIs | UT: psa_verify_hash
[Info] Executing tests from non-secure
[Check 1] Test psa_verify_hash - ECDSA KEY_PAIR SECP256R1 SHA-256
[Check 2] Test psa_verify_hash - EC public key
[Check 3] Test psa_verify_hash - Invalid key handle
[Check 4] Test psa_verify_hash - Zero as key handle

TEST RESULT: PASSED

******************************************

TEST: 243 | DESCRIPTION: Testing crypto key derivation APIs | UT: psa_raw_key_agreement
[Info] Executing tests from non-secure
[Check 1] Test psa_raw_key_agreement - Not a key agreement alg

TEST RESULT: PASSED

******************************************

TEST: 244 | DESCRIPTION: Testing crypto key management APIs | UT: psa_copy_key
[Info] Executing tests from non-secure
[Check 1] Test psa_copy_key - EC Public key

TEST RESULT: PASSED

******************************************

TEST: 245 | DESCRIPTION: Testing crypto hash functions APIs | UT: psa_hash_clone
[Info] Executing tests from non-secure
[Check 1] Test psa_hash_clone - SHA256 algorithm
[Check 2] Test psa_hash_clone - from an inactive source operation
[Check 3] Test psa_hash_clone - on an active target operation

TEST RESULT: PASSED

******************************************

TEST: 246 | DESCRIPTION: Testing crypto MAC APIs | UT: psa_mac_compute
[Info] Executing tests from non-secure
[Check 1] Test psa_mac_compute HMAC SHA 256

TEST RESULT: PASSED

******************************************

TEST: 247 | DESCRIPTION: Testing crypto MAC APIs | UT: psa_mac_verify
[Info] Executing tests from non-secure
[Check 1] Test psa_mac_verify HMAC SHA 256
[Check 2] Test psa_mac_verify - Incompactible HMAC for CMAC
[Check 3] Test psa_mac_verify - Invalid usage
[Check 4] Test psa_mac_verify - Truncated MAC too large
[Check 5] Test psa_mac_verify - Truncated MAC too small
[Check 6] Test psa_mac_verify - bad algorithm (unknown MAC algorithm)
[Check 7] Test psa_mac_verify - Invalid key type
[Check 8] Test psa_mac_verify small size buffer

TEST RESULT: PASSED

******************************************

TEST: 248 | DESCRIPTION: Testing crypto symmetric cipher APIs | UT: psa_cipher_encrypt
[Info] Executing tests from non-secure
No test available for the selected crypto configuration

TEST RESULT: SKIPPED (Skip Code=0x2d)

******************************************

TEST: 249 | DESCRIPTION: Testing crypto symmetric cipher APIs | UT: psa_cipher_decrypt
[Info] Executing tests from non-secure
No test available for the selected crypto configuration

TEST RESULT: SKIPPED (Skip Code=0x2d)

******************************************

TEST: 250 | DESCRIPTION: Testing crypto key management APIs | UT: psa_sign_message
[Info] Executing tests from non-secure
[Check 1] Test psa_sign_message - ECDSA SECP256R1 SHA-256
[Check 2] Test psa_sign_message - Invalid key handle
[Check 3] Test psa_sign_message - Zero as key handle

TEST RESULT: PASSED

******************************************

TEST: 251 | DESCRIPTION: Testing crypto key management APIs | UT: psa_verify_message
[Info] Executing tests from non-secure
[Check 1] Test psa_verify_message - ECDSA KEY_PAIR SECP256R1 SHA-256
[Check 2] Test psa_verify_message - ECDSA Public Key SECP256R1 SHA-256
[Check 3] Test psa_verify_message - Invalid key handle
[Check 4] Test psa_verify_message - Zero as key handle

TEST RESULT: PASSED

******************************************

TEST: 252 | DESCRIPTION: Testing crypto AEAD APIs | UT: psa_aead_encrypt_setup
[Info] Executing tests from non-secure
[Check 1] Test psa_aead_encrypt_setup - CCM - AES
[Check 2] Test psa_aead_encrypt_setup - CCM - AES - Tag length = 4
[Check 3] Test psa_aead_encrypt_setup - CCM - AES - Mismatched tag length
[Check 4] Test psa_aead_encrypt_setup - CCM - AES - Default Tag length

TEST RESULT: PASSED

******************************************

TEST: 253 | DESCRIPTION: Testing crypto AEAD APIs | UT: psa_aead_decrypt_setup
[Info] Executing tests from non-secure
[Check 1] Test psa_aead_decrypt_setup - CCM - AES
[Check 2] Test psa_aead_decrypt_setup - CCM - AES - Tag length = 4
[Check 3] Test psa_aead_decrypt_setup - CCM - AES - Mismatched tag length
[Check 4] Test psa_aead_decrypt_setup - CCM - AES - Default Tag length

TEST RESULT: PASSED

******************************************

TEST: 254 | DESCRIPTION: Testing crypto AEAD APIs | UT: psa_aead_generate_nonce
[Info] Executing tests from non-secure
[Check 1] Test psa_aead_generate_nonce - CCM
[Check 2] Test psa_aead_generate_nonce - CCM - Tag length = 4
[Check 3] Test psa_aead_generate_nonce - CCM - Small buffer size
[Check 4] Test psa_aead_generate_nonce - CCM - Uninitialized operation
[Check 5] Test psa_aead_generate_nonce - CCM - Decrypt operation

TEST RESULT: PASSED

******************************************

TEST: 255 | DESCRIPTION: Testing crypto AEAD APIs | UT: psa_aead_set_nonce
[Info] Executing tests from non-secure
[Check 1] Test psa_aead_set_nonce - Encrypt - CCM
[Check 2] Test psa_aead_set_nonce - Encrypt - CCM - Tag length = 4
[Check 3] Test psa_aead_set_nonce - Encrypt - CCM - Small nonce size
[Check 4] Test psa_aead_set_nonce - Encrypt - CCM - Large nonce size
[Check 5] Test psa_aead_set_nonce - Encrypt - CCM - Invalid operation state
[Check 6] Test psa_aead_set_nonce - Decrypt - CCM
[Check 7] Test psa_aead_set_nonce - Decrypt - CCM - Tag length = 4
[Check 8] Test psa_aead_set_nonce - Decrypt - CCM - Small nonce size
[Check 9] Test psa_aead_set_nonce - Decrypt - CCM - Large nonce size
[Check 10] Test psa_aead_set_nonce - Decrypt - CCM - Invalid operation state

TEST RESULT: PASSED

******************************************

TEST: 256 | DESCRIPTION: Testing crypto AEAD APIs | UT: psa_aead_set_lengths
[Info] Executing tests from non-secure
[Check 1] Test psa_aead_set_lengths - Encrypt - CCM
[Check 2] Test psa_aead_set_lengths - Encrypt - CCM - Tag length = 4
[Check 3] Test psa_aead_set_lengths - Encrypt - CCM - Zero ad_length
[Check 4] Test psa_aead_set_lengths - Encrypt - CCM - Zero plaintext_length
[Check 5] Test psa_aead_set_lengths - Encrypt - CCM - Invalid operation state
[Check 6] Test psa_aead_set_lengths - Decrypt - CCM
[Check 7] Test psa_aead_set_lengths - Decrypt - CCM - Tag length = 4
[Check 8] Test psa_aead_set_lengths - Decrypt - CCM - Zero ad_length
[Check 9] Test psa_aead_set_lengths - Decrypt - CCM - Zero plaintext_length
[Check 10] Test psa_aead_set_lengths - Decrypt - CCM - Invalid operation state

TEST RESULT: PASSED

******************************************

TEST: 257 | DESCRIPTION: Testing crypto AEAD APIs | UT: psa_aead_update_ad
[Info] Executing tests from non-secure
[Check 1] Test psa_aead_update_ad - Encrypt - CCM
[Check 2] Test psa_aead_update_ad - Encrypt - CCM - Tag length = 4
[Check 3] Test psa_aead_update_ad - Encrypt - CCM - Zero ad_length
[Check 4] Test psa_aead_update_ad - Encrypt - CCM - Zero plaintext_length
[Check 5] Test psa_aead_update_ad - Encrypt - CCM - Invalid operation state
[Check 6] Test psa_aead_update_ad - Encrypt - CCM - Overflow input length
[Check 7] Test psa_aead_update_ad - Decrypt - CCM
[Check 8] Test psa_aead_update_ad - Decrypt - CCM - Tag length = 4
[Check 9] Test psa_aead_update_ad - Decrypt - CCM - Zero ad_length
[Check 10] Test psa_aead_update_ad - Decrypt - CCM - Zero plaintext_length
[Check 11] Test psa_aead_update_ad - Decrypt - CCM - Invalid operation state
[Check 12] Test psa_aead_update_ad - Decrypt - CCM - Overflow input length

TEST RESULT: PASSED

******************************************

TEST: 258 | DESCRIPTION: Testing crypto AEAD APIs | UT: psa_aead_update
[Info] Executing tests from non-secure
[Check 1] Test psa_aead_update - Encrypt - CCM
[Check 2] Test psa_aead_update - Encrypt - CCM - Tag length = 4
[Check 3] Test psa_aead_update - Encrypt - CCM - Zero ad_length
[Check 4] Test psa_aead_update - Encrypt - CCM - Zero plaintext_length
[Check 5] Test psa_aead_update - Encrypt - CCM - Small buffer size
[Check 6] Test psa_aead_update - Encrypt - CCM - Less add data than specified
[Check 7] Test psa_aead_update - Encrypt - CCM - Overflow input length
[Check 8] Test psa_aead_update - Encrypt - CCM - Invalid operation state
[Check 9] Test psa_aead_update - Decrypt - CCM
[Check 10] Test psa_aead_update - Decrypt - CCM - Tag length = 4
[Check 11] Test psa_aead_update - Decrypt - CCM - Zero ad_length
[Check 12] Test psa_aead_update - Decrypt - CCM - Zero plaintext_length
[Check 13] Test psa_aead_update - Decrypt - CCM - Small buffer size
[Check 14] Test psa_aead_update - Decrypt - Less add data than specified
[Check 15] Test psa_aead_update - Decrypt - CCM - Overflow input length
[Check 16] Test psa_aead_update - Decrypt - CCM - Invalid operation state

TEST RESULT: PASSED

******************************************

TEST: 259 | DESCRIPTION: Testing crypto AEAD APIs | UT: psa_aead_finish
[Info] Executing tests from non-secure
[Check 1] Test psa_aead_finish - AES-CCM
[Check 2] Test psa_aead_finish - AES-CCM 24 bytes Tag length = 4
[Check 3] Test psa_aead_finish - Small buffer size
[Check 4] Test psa_aead_finish - Input length is less than plaintext length

TEST RESULT: PASSED

******************************************

TEST: 260 | DESCRIPTION: Testing crypto AEAD APIs | UT: psa_aead_abort
[Info] Executing tests from non-secure
[Check 1] Test psa_aead_abort - Encrypt - CCM - AES
[Check 2] Test psa_aead_abort - Decrypt - CCM - AES
[Check 3] Test psa_aead_abort with all initializations

TEST RESULT: PASSED

******************************************

TEST: 261 | DESCRIPTION: Testing crypto AEAD APIs | UT: psa_aead_verify
[Info] Executing tests from non-secure
[Check 1] Test psa_aead_verify - AES-CCM
[Check 2] Test psa_aead_verify - AES-CCM 24 bytes Tag length = 4
[Check 3] Test psa_aead_verify - Small buffer size
[Check 4] Test psa_aead_verify - Input length is less than plaintext length

TEST RESULT: PASSED

******************************************

************ Crypto Suite Report **********
TOTAL TESTS     : 61
TOTAL PASSED    : 51
TOTAL SIM ERROR : 0
TOTAL FAILED    : 0
TOTAL SKIPPED   : 10
******************************************

Entering standby..

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~