Defines valid options to be used by mcuxClEls_HashOption_t. More...
Macros | |
| #define | MCUXCLELS_HASH_INIT_ENABLE |
| Set this option at mcuxClEls_HashOption_t.hashini to initialize the hash. More... | |
| #define | MCUXCLELS_HASH_INIT_DISABLE |
| Set this option at mcuxClEls_HashOption_t.hashini to continue the hash. More... | |
| #define | MCUXCLELS_HASH_LOAD_ENABLE |
Set this option at mcuxClEls_HashOption_t.hashld to load the hash state from pDigest. More... | |
| #define | MCUXCLELS_HASH_LOAD_DISABLE |
| Set this option at mcuxClEls_HashOption_t.hashld to not load the hash state. More... | |
| #define | MCUXCLELS_HASH_OUTPUT_ENABLE |
Set this option at mcuxClEls_HashOption_t.hashoe to output the hash to pDigest. More... | |
| #define | MCUXCLELS_HASH_OUTPUT_DISABLE |
| Set this option at mcuxClEls_HashOption_t.hashoe to not output the hash. More... | |
| #define | MCUXCLELS_HASH_RTF_UPDATE_ENABLE |
| Set this option at mcuxClEls_HashOption_t.rtfupd to update the run-time fingerprint (only supported by #mcuxClEls_Hash_Async) More... | |
| #define | MCUXCLELS_HASH_RTF_UPDATE_DISABLE |
| Set this option at mcuxClEls_HashOption_t.rtfupd to not update the run-time fingerprint. More... | |
| #define | MCUXCLELS_HASH_RTF_OUTPUT_ENABLE |
| Set this option at mcuxClEls_HashOption_t.rtfoe to output the run-time fingerprint (only supported by #mcuxClEls_Hash_Async) More... | |
| #define | MCUXCLELS_HASH_RTF_OUTPUT_DISABLE |
| Set this option at mcuxClEls_HashOption_t.rtfoe to not output the run-time fingerprint. More... | |
| #define | MCUXCLELS_HASH_MODE_SHA_224 |
| Set this option at mcuxClEls_HashOption_t.hashmd to use the hash algorithm SHA-224. More... | |
| #define | MCUXCLELS_HASH_MODE_SHA_256 |
| Set this option at mcuxClEls_HashOption_t.hashmd to use the hash algorithm SHA-256. More... | |
| #define | MCUXCLELS_HASH_MODE_SHA_384 |
| Set this option at mcuxClEls_HashOption_t.hashmd to use the hash algorithm SHA-384. More... | |
| #define | MCUXCLELS_HASH_MODE_SHA_512 |
| Set this option at mcuxClEls_HashOption_t.hashmd to use the hash algorithm SHA-512. More... | |
| #define | MCUXCLELS_HASH_VALUE_MODE_SHA_224 |
| Set this option at #mcuxClEls_HashOption_t.word.value to use the hash algorithm SHA-224. More... | |
| #define | MCUXCLELS_HASH_VALUE_MODE_SHA_256 |
| Set this option at #mcuxClEls_HashOption_t.word.value to use the hash algorithm SHA-256. More... | |
| #define | MCUXCLELS_HASH_VALUE_MODE_SHA_384 |
| Set this option at #mcuxClEls_HashOption_t.word.value to use the hash algorithm SHA-384. More... | |
| #define | MCUXCLELS_HASH_VALUE_MODE_SHA_512 |
| Set this option at #mcuxClEls_HashOption_t.word.value to use the hash algorithm SHA-512. More... | |
Defines valid options to be used by mcuxClEls_HashOption_t.
| #define MCUXCLELS_HASH_INIT_ENABLE |
Set this option at mcuxClEls_HashOption_t.hashini to initialize the hash.
| #define MCUXCLELS_HASH_INIT_DISABLE |
Set this option at mcuxClEls_HashOption_t.hashini to continue the hash.
| #define MCUXCLELS_HASH_LOAD_ENABLE |
Set this option at mcuxClEls_HashOption_t.hashld to load the hash state from pDigest.
| #define MCUXCLELS_HASH_LOAD_DISABLE |
Set this option at mcuxClEls_HashOption_t.hashld to not load the hash state.
| #define MCUXCLELS_HASH_OUTPUT_ENABLE |
Set this option at mcuxClEls_HashOption_t.hashoe to output the hash to pDigest.
| #define MCUXCLELS_HASH_OUTPUT_DISABLE |
Set this option at mcuxClEls_HashOption_t.hashoe to not output the hash.
| #define MCUXCLELS_HASH_RTF_UPDATE_ENABLE |
Set this option at mcuxClEls_HashOption_t.rtfupd to update the run-time fingerprint (only supported by #mcuxClEls_Hash_Async)
| #define MCUXCLELS_HASH_RTF_UPDATE_DISABLE |
Set this option at mcuxClEls_HashOption_t.rtfupd to not update the run-time fingerprint.
| #define MCUXCLELS_HASH_RTF_OUTPUT_ENABLE |
Set this option at mcuxClEls_HashOption_t.rtfoe to output the run-time fingerprint (only supported by #mcuxClEls_Hash_Async)
| #define MCUXCLELS_HASH_RTF_OUTPUT_DISABLE |
Set this option at mcuxClEls_HashOption_t.rtfoe to not output the run-time fingerprint.
| #define MCUXCLELS_HASH_MODE_SHA_224 |
Set this option at mcuxClEls_HashOption_t.hashmd to use the hash algorithm SHA-224.
| #define MCUXCLELS_HASH_MODE_SHA_256 |
Set this option at mcuxClEls_HashOption_t.hashmd to use the hash algorithm SHA-256.
| #define MCUXCLELS_HASH_MODE_SHA_384 |
Set this option at mcuxClEls_HashOption_t.hashmd to use the hash algorithm SHA-384.
| #define MCUXCLELS_HASH_MODE_SHA_512 |
Set this option at mcuxClEls_HashOption_t.hashmd to use the hash algorithm SHA-512.
| #define MCUXCLELS_HASH_VALUE_MODE_SHA_224 |
Set this option at #mcuxClEls_HashOption_t.word.value to use the hash algorithm SHA-224.
| #define MCUXCLELS_HASH_VALUE_MODE_SHA_256 |
Set this option at #mcuxClEls_HashOption_t.word.value to use the hash algorithm SHA-256.
| #define MCUXCLELS_HASH_VALUE_MODE_SHA_384 |
Set this option at #mcuxClEls_HashOption_t.word.value to use the hash algorithm SHA-384.
| #define MCUXCLELS_HASH_VALUE_MODE_SHA_512 |
Set this option at #mcuxClEls_HashOption_t.word.value to use the hash algorithm SHA-512.