Defines all functions of mcuxClEcc. More...
Functions | |
| MCUX_CSSL_FP_PROTECTED_TYPE (mcuxClEcc_Status_t) mcuxClEcc_KeyGen(mcuxClSession_Handle_t pSession | |
| implements ECDSA key generation. More... | |
Defines all functions of mcuxClEcc.
| MCUX_CSSL_FP_PROTECTED_TYPE | ( | mcuxClEcc_Status_t | ) |
implements ECDSA key generation.
Deprecated type for mcuxClSession protected status codes.
Deprecated type for RSA protected status codes.
Deprecated type for error codes used by code-flow protected PKC component functions.
Deprecated type for error codes used by code-flow protected mcuxClMemory component functions.
Deprecated type for error codes used by code-flow protected Math component functions.
Deprecated type for Key component error codes, returned by functions with code-flow protection.
Deprecated type for ELS driver protected status codes.
Deprecated type for mcuxClEcc component return codes.
This function implements the protocol descriptor generation for Ed25519ctx, Ed25519ph, Ed448 and Ed448ph.
This function implements the EdDSA signature verification for Ed25519 and Ed448 as specified in rfc8032 (see Sections 5.1.7 and 5.2.7 of https://datatracker.ietf.org/doc/html/rfc8032).
This function implements the EdDSA signature generation for Ed25519 and Ed448 as specified in rfc8032 (see Sections 5.1.6 and 5.2.6 of https://datatracker.ietf.org/doc/html/rfc8032).
This function implements the EdDSA key pair generation for Ed25519 and Ed448 as specified in rfc8032 (see Sections 5.1.5 and 5.2.5 of https://datatracker.ietf.org/doc/html/rfc8032).
This function initializes an EdDSA mode descriptor for EdDSA key pair generation with private key input.
implements ECC key agreement according to rfc7748.
implements ECC key pair generation step for a MontDh key agreement according to rfc7748.
implements ECC point multiplication.
implements ECDSA signature verification.
implements ECDSA signature generation.
| MCUXCLECC_STATUS_OK | if private key and public key are generated successfully; |
| MCUXCLECC_STATUS_INVALID_PARAMS | if parameters are invalid; |
| MCUXCLECC_STATUS_RNG_ERROR | if random number (DRBG / PRNG) error (unexpected behavior); |
| MCUXCLECC_STATUS_FAULT_ATTACK | if fault attack (unexpected behavior) is detected. |
| MCUXCLECC_STATUS_OK | if signature is generated successfully; |
| MCUXCLECC_STATUS_INVALID_PARAMS | if parameters are invalid; |
| MCUXCLECC_STATUS_RNG_ERROR | if random number (DRBG / PRNG) error (unexpected behavior); |
| MCUXCLECC_STATUS_FAULT_ATTACK | if fault attack (unexpected behavior) is detected. |
| MCUXCLECC_STATUS_OK | if ECDSA Signature is valid; |
| MCUXCLECC_STATUS_INVALID_SIGNATURE | if ECDSA Signature is invalid; |
| MCUXCLECC_STATUS_INVALID_PARAMS | if parameters are invalid; |
| MCUXCLECC_STATUS_FAULT_ATTACK | if fault attack (unexpected behavior) is detected. |
This API performs elliptic curve point multiplication on the given elliptic curve in short Weierstrass form. This API does not check if the curve parameters and the given point are valid or not. Invalid curve parameters or point might cause the return of MCUXCLECC_STATUS_INVALID_PARAMS, invalid result, and unexpected behavior (e.g., the return of MCUXCLECC_STATUS_FAULT_ATTACK).
| [in] | pSession | pointer to mcuxClSession_Descriptor. |
| [in] | pParam | pointer to ECC point multiplication parameter structure. |
| MCUXCLECC_STATUS_OK | if point multiplication is calculated successfully, and the result is not the neutral point; |
| MCUXCLECC_STATUS_INVALID_PARAMS | if parameters are invalid; |
| MCUXCLECC_STATUS_NEUTRAL_POINT | if result is the neutral point; |
| MCUXCLECC_STATUS_FAULT_ATTACK | if fault attack (unexpected behavior) is detected. |
This API performs elliptic curve key generation of the private key and calculates corresponding public key for MontDh key agreement This API does not check if the curve parameters are correct. This API might return MCUXCLECC_STATUS_RNG_ERROR when RNG behave in unexpected way Unexpected behavior will return MCUXCLECC_STATUS_FAULT_ATTACK.
| [in] | pSession | mcuxClSession_Descriptor structure |
| [in] | type | type structure specifying requested key type to be generated. Also contains domain parameters |
| [in] | protection | #mcuxClKey_Protection structure |
| [out] | privKey | private key handling structure |
| [out] | pPrivData | buffer for private key of the MCUXCLECC_MONT_CURVE25519/448_SIZE_PRIVATEKEY length |
| [out] | pPrivDataLength | private key length |
| [out] | pubKey | public key handling structure |
| [out] | pPubData | buffer for public key x-coordinate of MCUXCLECC_MONT_CURVE25519/448_SIZE_PUBLICKEY length |
| [out] | pPubDataLength | public key x-coordinate length |
| MCUXCLECC_STATUS_OK | if key generation correctly calculate private and public keys, public key does not belong to the small subgroup. |
| MCUXCLECC_STATUS_RNG_ERROR | if RNG return an error. |
| MCUXCLECC_STATUS_FAULT_ATTACK | if fault attack (unexpected behavior) is detected. |
This API performs elliptic curve key agreement to compute shared secret between two parties using the function X25519 This API does not check if the curve parameters are correct. This API might return MCUXCLECC_STATUS_RNG_ERROR when RNG behave in unexpected way This API might return MCUXCLECC_STATUS_ERROR_SMALL_SUBGROUP if generated public key lies in the small subgroup Unexpected behavior will return MCUXCLECC_STATUS_FAULT_ATTACK.
| [in] | pSession | pointer to mcuxClSession_Descriptor. |
| [in] | key | private key handling structure |
| [in] | otherKey | public key handling structure |
| [out] | pOut | buffer for shared secret of length MCUXCLECC_MONT_CURVE25519/448_SIZE_SHAREDSECRET |
| [out] | pOutLength | shared secret length |
| MCUXCLECC_STATUS_OK | if key generation correctly calculate private and public keys, public key does not belong to the small subgroup. |
| MCUXCLECC_STATUS_RNG_ERROR | if RNG return an error. |
| MCUXCLECC_STATUS_ERROR_SMALL_SUBGROUP | if calculated public key lies in small subgroup. |
| MCUXCLECC_STATUS_FAULT_ATTACK | if fault attack (unexpected behavior) is detected. |
| [in] | pSession | Handle for the current CL session |
| [in/out] | mode Pointer to mode descriptor to be initialized for EdDSA key pair generation with private key input | |
| [in] | pPrivKey | Pointer to private key input |
| MCUXCLECC_STATUS_OK | EdDSA mode descriptor has been initialized successfully |
| MCUXCLECC_STATUS_FAULT_ATTACK | fault attack (unexpected behavior) is detected |
For an M byte private key d, which is either generated internally at random or passed as input, this function calculates the private key hash H(d)=(h0,...,h{2b-1}) and deduces and returns
This API does not check if the curve parameters are correct. This API might return MCUXCLECC_STATUS_RNG_ERROR when RNG behave in unexpected way Unexpected behavior will return MCUXCLECC_STATUS_FAULT_ATTACK.
| [in] | pSession | Handle for the current CL session |
| [in] | mode | Mode descriptor specifying the EdDSA GenerateKeyPair variant |
| [in/out] | privKey Key handle for the private key. | |
| [in/out] | pubKey Key handle for the public key. |
| MCUXCLECC_STATUS_OK | private key data and public key have been generated successfully |
| MCUXCLECC_STATUS_RNG_ERROR | random number generation (DRBG / PRNG) error (unexpected behavior) |
| MCUXCLECC_STATUS_FAULT_ATTACK | fault attack (unexpected behavior) is detected |
For given hash prefix prefix (either dom2(x, y) or dom4(x, y) according to the chosen EdDSA variant; see Sections 5.1 and 5.2 of https://datatracker.ietf.org/doc/html/rfc8032), a message digest m', i.e. either the message itself for PureEdDSA or the message hash for HashEdDSA (see Section 4 of https://datatracker.ietf.org/doc/html/rfc8032), the signing keys s and (hb,...,h{2b-1}) derived from the private key d (see mcuxClEcc_EdDSA_GenerateKeyPair) and a public key Qenc, this function calculates an EdDSA signature (Renc,S), where Renc and S are given by
- Renc = (r*G)enc - S = r+H(prefix||Renc||Qenc||m')*s mod n
where the secret scalar r is given by r=H(prefix||(hb,...,h{2b-1})||m') and G is the base point.
This API does not check if the curve parameters are correct. This API might return MCUXCLECC_STATUS_RNG_ERROR when RNG behave in unexpected way Unexpected behavior will return MCUXCLECC_STATUS_FAULT_ATTACK.
| [in] | pSession | Handle for the current CL session |
| [in] | key | Key handle for private key related data which a.o. references the secret signing keys s and (hb,...,h{2b-1}) as well as the public key Qenc. |
| [in] | mode | Mode descriptor specifying the EdDSA variant |
| [in] | pIn | Pointer to message digest m' |
| [in] | inSize | Size of message digest m' |
| [out] | pSignature | Pointer to buffer where the signature (Renc,S) will be stored |
| [out] | pSignatureSize | Will be set to the number of bytes of data that have been written to the pSignature buffer |
| MCUXCLECC_STATUS_OK | signature generation was successful |
| MCUXCLECC_STATUS_RNG_ERROR | random number generation (DRBG / PRNG) error (unexpected behavior) |
| MCUXCLECC_STATUS_FAULT_ATTACK | fault attack (unexpected behavior) is detected |
For given hash prefix prefix (either dom2(x, y) or dom4(x, y) according to the chosen EdDSA variant; see Sections 5.1 and 5.2 of https://datatracker.ietf.org/doc/html/rfc8032), a message digest m', i.e. either the message itself for PureEdDSA or the message hash for HashEdDSA (see Section 4 of https://datatracker.ietf.org/doc/html/rfc8032), and a public key Qenc, this function:
This API does not check if the curve parameters are correct. This API might return MCUXCLECC_STATUS_RNG_ERROR when RNG behave in unexpected way Unexpected behavior will return MCUXCLECC_STATUS_FAULT_ATTACK.
| [in] | pSession | Handle for the current CL session |
| [in] | key | Key handle for public key Qenc |
| [in] | mode | Mode descriptor specifying the EdDSA variant |
| [in] | pIn | Pointer to message digest m' |
| [in] | inSize | Size of message digest m' |
| [in] | pSignature | Pointer to buffer containing the signature (Renc,S) |
| [in] | signatureSize | Number of bytes of data in the pSignature buffer |
| MCUXCLECC_STATUS_OK | signature verification passed |
| MCUXCLECC_STATUS_INVALID_SIGNATURE | EdDSA signature is invalid |
| MCUXCLECC_STATUS_INVALID_PARAMS | input parameters are invalid |
| MCUXCLECC_STATUS_FAULT_ATTACK | fault attack (unexpected behavior) is detected |
| [in] | pSession | pointer to mcuxClSession_Descriptor |
| [in] | pDomainParams | Pointer to domain parameters of the used curve |
| [in] | pProtocolDescriptor | Protocol descriptor specifying the EdDSA variant |
| [in] | phflag | Option whether pre-hashing is enabled |
| [in] | pContext | User input context for the hash prefix |
| [in] | contextLen | Length of the context |
| MCUXCLECC_STATUS_OK | signature verification passed |
| MCUXCLECC_STATUS_FAULT_ATTACK | fault attack (unexpected behavior) is detected |
| const mcuxClEcc_PointMult_Param_t * pParam |
< [in] pointer to mcuxClSession_Descriptor.
< [in] pointer to ECDSA Key Generation parameter structure.
< [in] pointer to ECDSA Sign parameter structure.
< [in] pointer to ECDSA Verify parameter structure.