Defines all macros of mcuxClEls_Common. More...
Modules | |
| mcuxClEls_InterruptOptionEn_t | |
| Defines interrupt enable option values. | |
| mcuxClEls_InterruptOptionRst_t | |
| Defines interrupt reset option values. | |
| mcuxClEls_InterruptOptionSet_t | |
| Defines interrupt set option values. | |
| MCUXCLELS_ERROR_FLAGS_ | |
| Options for error flag clearing. | |
| MCUXCLELS_RESET_ | |
| Options for reset handling. | |
| MCUXCLELS_STATUS_PPROT_ | |
| Values for the privilege/security level of ELS commands. | |
| MCUXCLELS_STATUS_ECDSAVFY_ | |
| ECDSA verify check values. | |
| MCUXCLELS_STATUS_DRBGENTLVL_ | |
| Constants for Entropy quality of the current DRBG instance. | |
Macros | |
| #define | MCUXCLELS_API |
| Marks a function as a public API function of the mcuxClEls component. More... | |
| #define | MCUXCLELS_HW_VERSION |
| Compatible ELS hardware IP version for the CLNS release that this header is part of. More... | |
| #define | MCUXCLELS_DMA_READBACK_PROTECTION_TOKEN |
Defines all macros of mcuxClEls_Common.
| #define MCUXCLELS_API |
Marks a function as a public API function of the mcuxClEls component.
| #define MCUXCLELS_HW_VERSION |
Compatible ELS hardware IP version for the CLNS release that this header is part of.