Defines all functions of mcuxClEls_Ecc. More...
Functions | |
| MCUXCLELS_API | MCUX_CSSL_FP_PROTECTED_TYPE (mcuxClEls_Status_t) mcuxClEls_EccKeyGen_Async(mcuxClEls_EccKeyGenOption_t options |
| Generates an ECC key pair on the NIST P-256 curve. More... | |
Defines all functions of mcuxClEls_Ecc.
| MCUXCLELS_API MCUX_CSSL_FP_PROTECTED_TYPE | ( | mcuxClEls_Status_t | ) |
Generates an ECC key pair on the NIST P-256 curve.
Deprecated type for mcuxClSession protected status codes.
Deprecated type for RSA protected status codes.
Deprecated type for error codes used by code-flow protected PKC component functions.
Deprecated type for error codes used by code-flow protected mcuxClMemory component functions.
Deprecated type for error codes used by code-flow protected Math component functions.
Deprecated type for Key component error codes, returned by functions with code-flow protection.
Deprecated type for ELS driver protected status codes.
Deprecated type for mcuxClEcc component return codes.
Verifies an ECDSA signature of a given message.
Generates an ECDSA signature of a given message.
Performs a Diffie-Hellman key exchange with an internal ECC private key and an external ECC public key.
Before execution, ELS will wait until mcuxClEls_HwState_t.drbgentlvl == MCUXCLELS_STATUS_DRBGENTLVL_HIGH. This can lead to a delay if the DRBG is in a state with less security strength at the time of the call.
Call #mcuxClEls_WaitForOperation to complete the operation. The public key will be stored in the standard ANSI X9.62 byte order (big-endian).
| [in] | options | The command options. For more information, see mcuxClEls_EccKeyGenOption_t. |
| [in] | signingKeyIdx | The index of the key to sign the generated public key. |
| [in] | privateKeyIdx | Output key index. |
| [in] | generatedKeyProperties | The desired key properties of the generated key. |
| [in] | pRandomData | Random data provided by the user. |
| [out] | pPublicKey | Pointer to the memory area which receives the public key and optionally the key signature. |
options.kgsign == MCUXCLELS_ECC_PUBLICKEY_SIGN_DISABLE signingKeyIdx is ignored. options.kgsrc == MCUXCLELS_ECC_OUTPUTKEY_DETERMINISTIC privateKeyIdx also defines the key index of the source key material. The source key material will be overwritten by the output public key. options.kgsign_rnd == MCUXCLELS_ECC_NO_RANDOM_DATA pRandomData is ignored. pPublicKey must be aligned on a 4-byte boundary. | MCUXCLELS_STATUS_SW_INVALID_PARAM | if invalid parameters were specified |
| MCUXCLELS_STATUS_SW_CANNOT_INTERRUPT | if a running operation prevented the request |
| MCUXCLELS_STATUS_OK_WAIT | on successful request |
Before execution, ELS will wait until mcuxClEls_HwState_t.drbgentlvl == MCUXCLELS_STATUS_DRBGENTLVL_LOW. This can lead to a delay if the DRBG is in a state with less security strength at the time of the call.
Call #mcuxClEls_WaitForOperation to complete the operation. The public key must be stored in the standard ANSI X9.62 byte order (big-endian).
| [in] | privateKeyIdx | The private key index. |
| [in] | pPublicKey | Pointer to the public key of a third party. |
| [in] | sharedSecretIdx | The index in the ELS keystore that receives the shared secret that is generated by the ECDH operation. |
| [in] | sharedSecretProperties | The desired key properties of the shared secret. |
pPublicKey | MCUXCLELS_STATUS_SW_INVALID_PARAM | if invalid parameters were specified |
| MCUXCLELS_STATUS_SW_CANNOT_INTERRUPT | if a running operation prevented the request |
| MCUXCLELS_STATUS_OK_WAIT | on successful request |
The curve is NIST P-256. The message hash, must be stored in the standard ANSI X9.62 format. If the message is provided in plain, no prior conversion is necessary. The signature will be stored in the standard ANSI X9.62 byte order (big-endian).
Before execution, ELS will wait until mcuxClEls_HwState_t.drbgentlvl == MCUXCLELS_STATUS_DRBGENTLVL_HIGH. This can lead to a delay if the DRBG is in a state with less security strength at the time of the call.
Call #mcuxClEls_WaitForOperation to complete the operation.
| [in] | options | The command options. For more information, see mcuxClEls_EccSignOption_t. |
| [in] | keyIdx | The private key index. |
| [in] | pInputHash | The hash of the message to sign in X9.62 format. |
| [in] | pInputMessage | The message to sign. |
| [in] | inputMessageLength | Size of pInputMessage in bytes. |
| [out] | pOutput | Pointer to the memory area which receives the generated signature in X9.62 format. (64 bytes) |
options.echashchl == MCUXCLELS_ECC_HASHED pInputHash is used, and it must be aligned on a 4-byte boundary. pInputMessage is ignored. options.echashchl == MCUXCLELS_ECC_NOT_HASHED pInputHash is ignored. pInputMessage and inputMessageLength are used. pOptput must be aligned on a 4-byte boundary. | MCUXCLELS_STATUS_SW_INVALID_PARAM | if invalid parameters were specified |
| MCUXCLELS_STATUS_SW_CANNOT_INTERRUPT | if a running operation prevented the request |
| MCUXCLELS_STATUS_OK_WAIT | on successful request |
The curve is NIST P-256. The message hash, must be stored in the standard ANSI X9.62 format. If the message is provided in plain, no prior conversion is necessary. The signature and public key must be stored in the standard ANSI X9.62 byte order (big-endian).
Before execution, ELS will wait until mcuxClEls_HwState_t.drbgentlvl == MCUXCLELS_STATUS_DRBGENTLVL_LOW. This can lead to a delay if the DRBG is in a state with less security strength at the time of the call.
Call #mcuxClEls_WaitForOperation to complete the operation.
| [in] | options | The command options. For more information, see mcuxClEls_EccVerifyOption_t. |
| [in] | pInputHash | The hash of the signed message in X9.62 format. |
| [in] | pInputMessage | The message to sign. |
| [in] | inputMessageLength | Size of pInputMessage in bytes. |
| [in] | pSignatureAndPubKey | Pointer to the memory area which contains the concatenation of the signature and the public key. |
| [out] | pOutput | Pointer to the memory area which will receive the recalculated value of the R component in case of a successful signature verification. |
options.echashchl == MCUXCLELS_ECC_HASHED pInputHash is used, and it must be aligned on a 4-byte boundary. pInputMessage is ignored. options.echashchl == MCUXCLELS_ECC_NOT_HASHED pInputHash is ignored. pInputMessage and inputMessageLength are used. pSignatureAndPubKey pOutput pSignatureAndPublicKey. | MCUXCLELS_STATUS_SW_INVALID_PARAM | if invalid parameters were specified |
| MCUXCLELS_STATUS_SW_CANNOT_INTERRUPT | if a running operation prevented the request |
| MCUXCLELS_STATUS_OK_WAIT | on successful request |