Defines all macros of mcuxClEls_Hash. More...
Modules | |
| MCUXCLELS_HASH_ | |
| Defines valid options to be used by mcuxClEls_HashOption_t. | |
| MCUXCLELS_HASH_BLOCK_SIZE_ | |
| Defines block sizes used by the supported hash algorithms. | |
| MCUXCLELS_HASH_STATE_SIZE_ | |
| Defines the intermediate state sizes of the supported hash algorithms. | |
| MCUXCLELS_HASH_OUTPUT_SIZE_ | |
| Defines the output sizes of the supported hash algorithms (do not use for allocation) | |
| #define | MCUXCLELS_HASH_RTF_OUTPUT_SIZE |
Defines all macros of mcuxClEls_Hash.
| #define MCUXCLELS_HASH_RTF_OUTPUT_SIZE |
Size of run-time fingerprint appended to the hash in pDigest in bytes, if MCUXCLELS_HASH_RTF_OUTPUT_ENABLE was specified