Defines all functions of mcuxClKey. More...
Functions | |
| MCUX_CSSL_FP_PROTECTED_TYPE (mcuxClKey_Status_t) mcuxClKey_init(mcuxClSession_Handle_t pSession | |
| Initializes a key handle. More... | |
Variables | |
| mcuxClKey_Handle_t | key |
| mcuxClKey_Handle_t mcuxClKey_Type_t | type |
| mcuxClKey_Handle_t mcuxClKey_Type_t mcuxCl_InputBuffer_t | pKeyData |
| mcuxClKey_Handle_t mcuxClKey_Type_t mcuxCl_InputBuffer_t uint32_t | keyDataLength |
| mcuxClKey_Handle_t | privKey |
| mcuxClKey_Handle_t mcuxClKey_Handle_t | pubKey |
| mcuxClKey_Handle_t mcuxClKey_Protection_t | protection |
| mcuxClKey_Handle_t mcuxClKey_Protection_t mcuxCl_Buffer_t | pAuxData |
| mcuxClKey_Handle_t mcuxClKey_Protection_t mcuxCl_Buffer_t mcuxClKey_Handle_t | parentKey |
| mcuxClKey_Handle_t uint32_t | dstSlot |
| mcuxClKey_Handle_t uint32_t * | dstData |
| mcuxClEls_KeyProp_t * | key_properties |
Defines all functions of mcuxClKey.
| MCUX_CSSL_FP_PROTECTED_TYPE | ( | mcuxClKey_Status_t | ) |
Initializes a key handle.
Deprecated type for mcuxClSession protected status codes.
Deprecated type for RSA protected status codes.
Deprecated type for error codes used by code-flow protected PKC component functions.
Deprecated type for error codes used by code-flow protected mcuxClMemory component functions.
Deprecated type for error codes used by code-flow protected Math component functions.
Deprecated type for Key component error codes, returned by functions with code-flow protection.
Deprecated type for ELS driver protected status codes.
Deprecated type for mcuxClEcc component return codes.
Set the requested key properties of the destination key.
Flush key from destination which can be a key slot of coprocessor or memory buffer.
Load key into destination memory buffer.
Load key into destination key slot of a coprocessor.
Configures they protection mechanism for to the given key handle.
Establishes a key pair link between a private and public key handle.
Initializes a key handle with default protection values.
| [in] | pSession | Session handle to provide session dependent information |
| [in,out] | key | Key handle that will be initialized |
| [in] | type | Define which key type shall be initialized |
| [in] | pKeyData | Provide pointer to source data of the key. This can be a pointer to a plain key buffer, a share, or a key blob. The protection function defines the purpose of this parameter |
| [in] | keyDataLength | Length of the provided key data pKeyData |
| MCUXCLKEY_STATUS_ERROR | on unsuccessful operation |
| MCUXCLKEY_STATUS_OK | on successful operation |
| [in] | pSession | Session handle to provide session dependent information |
| [in,out] | privKey | Key handle of private key |
| [in,out] | pubKey | Key handle of public key |
| MCUXCLKEY_STATUS_ERROR | on unsuccessful operation |
| MCUXCLKEY_STATUS_OK | on successful operation |
| [in] | pSession | Session handle to provide session dependent information |
| [in,out] | key | Key handle that will be configured |
| [in] | protection | Define the protection and flush mechanism that shall be used with this key |
| [in] | pAuxData | Provide pointer to additional data the protection function may use |
| [in] | parentKey | Provide parent key information in case it exists. The protection function defines the purpose of this parameter |
| MCUXCLKEY_STATUS_ERROR | on unsuccessful operation |
| MCUXCLKEY_STATUS_OK | on successful operation |
| [in] | pSession | Session handle to provide session dependent information |
| [in] | key | Key handle that provides information to load the key |
| [out] | dstSlot | Provide destination key slot in case the key has to loaded to a key slot. The protection function defines the purpose of this parameter |
| MCUXCLKEY_STATUS_ERROR | on unsuccessful operation |
| MCUXCLKEY_STATUS_OK | on successful operation |
| [in] | pSession | Session handle to provide session dependent information |
| [in] | key | Key handle that provides information to load the key |
| [out] | dstData | Provide pointer to destination key memory in case the key has to be loaded to memory. The protection function defines the purpose of this parameter |
| MCUXCLKEY_STATUS_ERROR | on unsuccessful operation |
| MCUXCLKEY_STATUS_OK | on successful operation |
| [in] | pSession | Session handle to provide session dependent information |
| [in] | key | Key handle that provides information to flush the key |
| MCUXCLKEY_STATUS_ERROR | on unsuccessful operation |
| MCUXCLKEY_STATUS_OK | on successful operation |
| [in,out] | key | key handle that provides information to flush the key |
| [in] | key_properties | Pointer to the requested key properties of the destination key. Will be set in key->container.pAuxData |
| MCUXCLKEY_STATUS_ERROR | on unsuccessful operation |
| MCUXCLKEY_STATUS_OK | on successful operation |