These macros implement endianess management on integers.
More...
These macros implement endianess management on integers.
◆ mcuxClMemory_StoreLittleEndian32
| #define mcuxClMemory_StoreLittleEndian32 |
( |
|
destination, |
|
|
|
value |
|
) |
| |
Converts a 32-bit unsigned integer to a little-endian order uint8_t array .
- Note
- Implementation is platform independent.
- Parameters
-
| [out] | destination | pointer to a 4 byte buffer were 32-bit integer in little-endian will be encoded. |
| [in] | value | pointer to the 32-bit integer to be encoded. |
◆ mcuxClMemory_StoreBigEndian32
| #define mcuxClMemory_StoreBigEndian32 |
( |
|
destination, |
|
|
|
value |
|
) |
| |
Converts a 32-bit unsigned integer to a big-endian order uint8_t array.
- Note
- Implementation is platform independent.
- Parameters
-
| [in] | source | pointer to a 4 byte big-endian order uint8_t buffer that will be converted to an unsigned integer |
◆ mcuxClMemory_LoadLittleEndian32
| #define mcuxClMemory_LoadLittleEndian32 |
( |
|
source | ) |
|
Converts a little-endian order uint8_t array to a 32-bit unsigned integer.
- Note
- Implementation is platform independent.
- Parameters
-
| [in] | source | pointer to a 4 byte little-endian order uint8_t buffer that will be converted to an unsigned integer |
◆ mcuxClMemory_LoadBigEndian32
| #define mcuxClMemory_LoadBigEndian32 |
( |
|
source | ) |
|
Converts a big-endian order uint8_t array to a 32-bit unsigned integer.
- Parameters
-
| [in] | destination | pointer to a 4 byte buffer were 32-bit integer in big-endian will be decoded. |
- Returns
- a 32-bit unsigned integer
◆ MCUXCLMEMORY_SWITCH_4BYTE_ENDIANNESS
| #define MCUXCLMEMORY_SWITCH_4BYTE_ENDIANNESS |
( |
|
input | ) |
|
MACRO that switches byte endianness of given CPU word.
- Parameters
-
| [in] | input | a 32-bit unsigned integer whose endianness will be reversed. |