Defines all functions of mcuxClSession. More...
Functions | |
| MCUX_CSSL_FP_PROTECTED_TYPE (mcuxClSession_Status_t) mcuxClSession_init(mcuxClSession_Handle_t pSession | |
| Initialize a Crypto Library session. More... | |
Variables | |
| uint32_t *const | pCpuWaBuffer |
| uint32_t *const uint32_t | cpuWaLength |
| uint32_t *const uint32_t uint32_t *const | pPkcWaBuffer |
| uint32_t *const uint32_t uint32_t *const uint32_t | pkcWaLength |
| uint8_t *const | pRtf |
| uint8_t *const mcuxClSession_Rtf_t | RtfOptions |
Defines all functions of mcuxClSession.
| MCUX_CSSL_FP_PROTECTED_TYPE | ( | mcuxClSession_Status_t | ) |
Initialize a Crypto Library session.
Deprecated type for mcuxClSession protected status codes.
Deprecated type for RSA protected status codes.
Deprecated type for error codes used by code-flow protected PKC component functions.
Deprecated type for error codes used by code-flow protected mcuxClMemory component functions.
Deprecated type for error codes used by code-flow protected Math component functions.
Deprecated type for Key component error codes, returned by functions with code-flow protection.
Deprecated type for ELS driver protected status codes.
Deprecated type for mcuxClEcc component return codes.
Destroy a Crypto Library session.
Clean up a Crypto Library session.
Set the RTF option in a Crypto Library session.
| pSession | Session to be initialized. |
| pCpuWaBuffer | Pointer to buffer to be used as workarea for CPU operations. This pointer shall be CPU-word aligned. |
| cpuWaLength | Size (in bytes) of the workarea for CPU operations. The size shall be a multiple of CPU wordsize. |
| pPkcWaBuffer | Pointer to buffer to be used as workarea for PKC operations. This pointer shall be PKC-word aligned. |
| pkcWaLength | Size (in bytes) of the workarea for PKC operations. The size shall be a multiple of CPU wordsize. |
| MCUXCLSESSION_STATUS_OK | Session has been initialized successfully |
| MCUXCLSESSION_STATUS_ERROR | Error occurred during session initializing. |
| pSession | Session to be initialized. |
| pRtf | buffer to store the rtf result. |
| RtfOptions | Options to define RTF processing. |
This function will (securely) cleanup the session, which will still be usable afterwards.
| pSession | Session to be cleaned. |
This function will (securely) cleanup the session, including uninitialization etc. The session will no longer be usable afterwards.
| pSession | Session to be destroyed. |