Top-level API of the mcuxClCipher component. More...
#include <mcuxClConfig.h>#include <mcuxClSession_Types.h>#include <mcuxClKey_Types.h>#include <mcuxClCipher_Types.h>#include <mcuxClCore_Platform.h>#include <mcuxClCore_Buffer.h>Go to the source code of this file.
Functions | |
| MCUX_CSSL_FP_PROTECTED_TYPE (mcuxClCipher_Status_t) mcuxClCipher_crypt(mcuxClSession_Handle_t session | |
| One-shot encryption/decryption function. More... | |
Variables | |
| mcuxClKey_Handle_t | key |
| mcuxClKey_Handle_t mcuxClCipher_Mode_t | mode |
| mcuxClKey_Handle_t mcuxClCipher_Mode_t mcuxCl_InputBuffer_t | pIv |
| mcuxClKey_Handle_t mcuxClCipher_Mode_t mcuxCl_InputBuffer_t uint32_t | ivLength |
| mcuxClKey_Handle_t mcuxClCipher_Mode_t mcuxCl_InputBuffer_t uint32_t mcuxCl_InputBuffer_t | pIn |
| mcuxClKey_Handle_t mcuxClCipher_Mode_t mcuxCl_InputBuffer_t uint32_t mcuxCl_InputBuffer_t uint32_t | inLength |
| mcuxClKey_Handle_t mcuxClCipher_Mode_t mcuxCl_InputBuffer_t uint32_t mcuxCl_InputBuffer_t uint32_t mcuxCl_Buffer_t | pOut |
| mcuxClKey_Handle_t mcuxClCipher_Mode_t mcuxCl_InputBuffer_t uint32_t mcuxCl_InputBuffer_t uint32_t mcuxCl_Buffer_t uint32_t *const | pOutLength |
| mcuxClCipher_Context_t *const | pContext |
Top-level API of the mcuxClCipher component.