ELS header for Authenticated Encryption with Associated Data (AEAD). More...
Go to the source code of this file.
Data Structures | |
| union | mcuxClEls_AeadOption_t |
| Command option bit field for #mcuxClEls_Aead_Init_Async, #mcuxClEls_Aead_UpdateAad_Async, #mcuxClEls_Aead_UpdateData_Async and #mcuxClEls_Aead_Finalize_Async. More... | |
Macros | |
| #define | MCUXCLELS_AEAD_ENCRYPT |
| Set mcuxClEls_AeadOption_t.dcrpt to this value to encrypt data. More... | |
| #define | MCUXCLELS_AEAD_DECRYPT |
| Set mcuxClEls_AeadOption_t.dcrpt to this value to decrypt data. More... | |
| #define | MCUXCLELS_AEAD_STATE_IN_DISABLE |
| Set mcuxClEls_AeadOption_t.acpsie to this value to load the GCM state from ELS. More... | |
| #define | MCUXCLELS_AEAD_STATE_IN_ENABLE |
| Set mcuxClEls_AeadOption_t.acpsie to this value to load the GCM state from the context. More... | |
| #define | MCUXCLELS_AEAD_LASTINIT_TRUE |
| Set mcuxClEls_AeadOption_t.lastinit to this value if this is the last call to init. More... | |
| #define | MCUXCLELS_AEAD_LASTINIT_FALSE |
| Set mcuxClEls_AeadOption_t.lastinit to this value if this is not the last call to init. More... | |
| #define | MCUXCLELS_AEAD_EXTERN_KEY |
| Set mcuxClEls_AeadOption_t.extkey to this value to use an external key. More... | |
| #define | MCUXCLELS_AEAD_INTERN_KEY |
| Set mcuxClEls_AeadOption_t.extkey to this value to use a key from the ELS keystore. More... | |
| #define | MCUXCLELS_AEAD_ACPMOD_INIT |
| Set mcuxClEls_AeadOption_t.acpmod to this value for Init mode. For internal use. More... | |
| #define | MCUXCLELS_AEAD_ACPMOD_AADPROC |
| Set mcuxClEls_AeadOption_t.acpmod to this value for Process Additional Authenticated Data mode. For internal use. More... | |
| #define | MCUXCLELS_AEAD_ACPMOD_MSGPROC |
| Set mcuxClEls_AeadOption_t.acpmod to this value for Process Message mode. For internal use. More... | |
| #define | MCUXCLELS_AEAD_ACPMOD_FINAL |
| Set mcuxClEls_AeadOption_t.acpmod to this value for Finalize mode. For internal use. More... | |
| #define | MCUXCLELS_AEAD_STATE_OUT_ENABLE |
| Set mcuxClEls_AeadOption_t.acpsoe to this value to save the state to the context. For internal use. More... | |
| #define | MCUXCLELS_AEAD_IV_BLOCK_SIZE |
| #define | MCUXCLELS_AEAD_AAD_BLOCK_SIZE |
| AES-GCM AAD Granularity: 128 bit (16 bytes) More... | |
| #define | MCUXCLELS_AEAD_TAG_SIZE |
| tag size: Tag generation supports only a 128 bit wide tag (16 bytes) More... | |
| #define | MCUXCLELS_AEAD_CONTEXT_SIZE |
| context size: 512 bit (64 bytes) + 16 bytes for finalize More... | |
Functions | |
| MCUXCLELS_API | MCUX_CSSL_FP_PROTECTED_TYPE (mcuxClEls_Status_t) mcuxClEls_Aead_Init_Async(mcuxClEls_AeadOption_t options |
| AES-GCM initialization. More... | |
Variables | |
| MCUXCLELS_API mcuxClEls_KeyIndex_t | keyIdx |
| MCUXCLELS_API mcuxClEls_KeyIndex_t uint8_t const * | pKey |
| MCUXCLELS_API mcuxClEls_KeyIndex_t uint8_t const size_t | keyLength |
| MCUXCLELS_API mcuxClEls_KeyIndex_t uint8_t const size_t uint8_t const * | pIV |
| MCUXCLELS_API mcuxClEls_KeyIndex_t uint8_t const size_t uint8_t const size_t | ivLength |
| MCUXCLELS_API mcuxClEls_KeyIndex_t uint8_t const size_t uint8_t const size_t uint8_t * | pAeadCtx |
| MCUXCLELS_API mcuxClEls_KeyIndex_t uint8_t const size_t uint8_t const * | pAad |
| MCUXCLELS_API mcuxClEls_KeyIndex_t uint8_t const size_t uint8_t const size_t | aadLength |
| MCUXCLELS_API mcuxClEls_KeyIndex_t uint8_t const size_t uint8_t const * | pInput |
| MCUXCLELS_API mcuxClEls_KeyIndex_t uint8_t const size_t uint8_t const size_t | inputLength |
| MCUXCLELS_API mcuxClEls_KeyIndex_t uint8_t const size_t uint8_t const size_t uint8_t * | pOutput |
| MCUXCLELS_API mcuxClEls_KeyIndex_t uint8_t const size_t size_t size_t | dataLength |
| MCUXCLELS_API mcuxClEls_KeyIndex_t uint8_t const size_t size_t size_t uint8_t * | pTag |
ELS header for Authenticated Encryption with Associated Data (AEAD).
This header exposes functions that enable using the ELS for Authenticated Encryption with Associated Data (AEAD). The AEAD algorithm supported by ELS is AES in Galois/Counter Mode (GCM), as described in NIST Special Publication 800-38D.