ELS header for elliptic curve cryptography This header exposes functions that enable using the ELS for elliptic curve cryptography. More...
Go to the source code of this file.
Data Structures | |
| union | mcuxClEls_EccSignOption_t |
| Command option bit field for #mcuxClEls_EccSign_Async Bit field to configure #mcuxClEls_EccSign_Async. More... | |
| union | mcuxClEls_EccVerifyOption_t |
| Command option bit field for #mcuxClEls_EccVerify_Async Bit field to configure mcuxClEls_EccVerifyOption_t. More... | |
| union | mcuxClEls_EccKeyGenOption_t |
| Command option bit field for #mcuxClEls_EccKeyGen_Async Bit field to configure mcuxClEls_EccKeyGenOption_t. More... | |
| union | mcuxClEls_EccKeyExchOption_t |
| Command option bit field for #mcuxClEls_EccKeyExchange_Async, for internal use only. More... | |
Macros | |
| #define | MCUXCLELS_ECC_VALUE_HASHED |
| Set this option at mcuxClEls_EccSignOption_t.value or mcuxClEls_EccVerifyOption_t.value to specify input is the hash of the message. More... | |
| #define | MCUXCLELS_ECC_VALUE_NOT_HASHED |
| Set this option at mcuxClEls_EccSignOption_t.value or mcuxClEls_EccVerifyOption_t.value to specify input is the plain message. More... | |
| #define | MCUXCLELS_ECC_VALUE_RTF |
| Set this option at mcuxClEls_EccSignOption_t.value to include the RTF in the signature, only for mcuxClEls_EccSignOption_t. More... | |
| #define | MCUXCLELS_ECC_VALUE_NO_RTF |
| Set this option at mcuxClEls_EccSignOption_t.value to not include the RTF in the signature, only for mcuxClEls_EccSignOption_t. More... | |
| #define | MCUXCLELS_KEYGEN_VALUE_SIGN_PUBLICKEY |
| Set this option at mcuxClEls_EccKeyGenOption_t.value to sign the public key. More... | |
| #define | MCUXCLELS_KEYGEN_VALUE_TYPE_SIGN |
| Set this option at mcuxClEls_EccKeyGenOption_t.value to specify output key will be a signing key usable by #mcuxClEls_EccSign_Async. More... | |
| #define | MCUXCLELS_KEYGEN_VALUE_TYPE_KEYEXCHANGE |
| Set this option at mcuxClEls_EccKeyGenOption_t.value to specify output key will be a Diffie Helman key usable by #mcuxClEls_EccKeyExchange_Async. More... | |
| #define | MCUXCLELS_KEYGEN_VALUE_DETERMINISTIC |
| Set this option at mcuxClEls_EccKeyGenOption_t.value to specify output key is deterministic. More... | |
| #define | MCUXCLELS_KEYGEN_VALUE_RANDOM |
| Set this option at mcuxClEls_EccKeyGenOption_t.value to specify output key is random. More... | |
| #define | MCUXCLELS_KEYGEN_VALUE_GEN_PUB_KEY |
| Set this option at mcuxClEls_EccKeyGenOption_t.value to generate a public key. More... | |
| #define | MCUXCLELS_KEYGEN_VALUE_NO_PUB_KEY |
| Set this option at mcuxClEls_EccKeyGenOption_t.value to not generate a public key. More... | |
| #define | MCUXCLELS_KEYGEN_VALUE_NO_RANDOM_DATA |
| Set this option at mcuxClEls_EccKeyGenOption_t.value to not use random data for signing the public key. More... | |
| #define | MCUXCLELS_KEYGEN_VALUE_USE_RANDOM_DATA |
| Set this option at mcuxClEls_EccKeyGenOption_t.value to use random data for signing the public key. More... | |
| #define | MCUXCLELS_ECC_HASHED |
| Set this option at mcuxClEls_EccSignOption_t.echashchl or mcuxClEls_EccVerifyOption_t.echashchl to specify input is the hash of the message. More... | |
| #define | MCUXCLELS_ECC_NOT_HASHED |
| Set this option at mcuxClEls_EccSignOption_t.echashchl or mcuxClEls_EccVerifyOption_t.echashchl to specify input is the plain message. More... | |
| #define | MCUXCLELS_ECC_RTF |
| Set this option at mcuxClEls_EccSignOption_t.signrtf to include the RTF in the signature. More... | |
| #define | MCUXCLELS_ECC_NO_RTF |
| Set this option at mcuxClEls_EccSignOption_t.signrtf to not include the RTF in the signature. More... | |
| #define | MCUXCLELS_ECC_PUBLICKEY_SIGN_ENABLE |
| Set this option at mcuxClEls_EccKeyGenOption_t.kgsign to sign the public key (signature will be concatenated to the output public key) More... | |
| #define | MCUXCLELS_ECC_PUBLICKEY_SIGN_DISABLE |
| Set this option at mcuxClEls_EccKeyGenOption_t.kgsign to not sign the public key. More... | |
| #define | MCUXCLELS_ECC_OUTPUTKEY_SIGN |
| Set this option at mcuxClEls_EccKeyGenOption_t.kgtypedh to specify output key will be a signing key usable by #mcuxClEls_EccSign_Async. More... | |
| #define | MCUXCLELS_ECC_OUTPUTKEY_KEYEXCHANGE |
| Set this option at mcuxClEls_EccKeyGenOption_t.kgtypedh to specify output key will be a Diffie Helman key usable by #mcuxClEls_EccKeyExchange_Async. More... | |
| #define | MCUXCLELS_ECC_OUTPUTKEY_DETERMINISTIC |
| Set this option at mcuxClEls_EccKeyGenOption_t.kgsrc to specify output key is deterministic. More... | |
| #define | MCUXCLELS_ECC_OUTPUTKEY_RANDOM |
| Set this option at mcuxClEls_EccKeyGenOption_t.kgsrc to specify output key is random. More... | |
| #define | MCUXCLELS_ECC_GEN_PUBLIC_KEY |
| Set this option at mcuxClEls_EccKeyGenOption_t.skip_pbk to generate a public key. More... | |
| #define | MCUXCLELS_ECC_SKIP_PUBLIC_KEY |
| Set this option at mcuxClEls_EccKeyGenOption_t.skip_pbk to not generate a public key. More... | |
| #define | MCUXCLELS_ECC_NO_RANDOM_DATA |
| Set this option at mcuxClEls_EccKeyGenOption_t.kgsign_rnd to not include user provided random data for the signature. More... | |
| #define | MCUXCLELS_ECC_INCLUDE_RANDOM_DATA |
| Set this option at mcuxClEls_EccKeyGenOption_t.kgsign_rnd to include user provided random data for the signature. More... | |
| #define | MCUXCLELS_ECC_REVERSEFETCH_ENABLE |
| Reverse Fetch enabled. For internal use. More... | |
| #define | MCUXCLELS_ECC_REVERSEFETCH_DISABLE |
| Reverse Fetch disabled. For internal use. More... | |
| #define | MCUXCLELS_ECC_PUBLICKEY_SIZE |
| Size of the public key. More... | |
| #define | MCUXCLELS_ECC_SIGNATURE_SIZE |
| Size of the signature. More... | |
| #define | MCUXCLELS_ECC_SIGNATURE_R_SIZE |
| Size of the signature part r. More... | |
Typedefs | |
| typedef uint8_t | mcuxClEls_EccByte_t |
| Data type for ECC parameters in ELS format. More... | |
Functions | |
| MCUXCLELS_API | MCUX_CSSL_FP_PROTECTED_TYPE (mcuxClEls_Status_t) mcuxClEls_EccKeyGen_Async(mcuxClEls_EccKeyGenOption_t options |
| Generates an ECC key pair on the NIST P-256 curve. More... | |
ELS header for elliptic curve cryptography This header exposes functions that enable using the ELS for elliptic curve cryptography.
All functions operate on the NIST P-256 curve. The ECC operations supported are: