TLS key derivation example. More...
#include <mcuxClEls.h>#include <mcuxClMemory.h>#include <mcuxCsslFlowProtection.h>#include <mcuxClCore_FunctionIdentifiers.h>#include <mcuxClCore_Examples.h>#include <mcuxClExample_ELS_Helper.h>#include <mcuxClExample_ELS_Key_Helper.h>Functions | |
| MCUXCLEXAMPLE_FUNCTION (mcuxClEls_Tls_Master_Key_Session_Keys_example) | |
| Performs key derivation for TLS protocol. More... | |
Variables | |
| static mcuxClEls_EccByte_t | ecc_public_key_client [MCUXCLELS_ECC_PUBLICKEY_SIZE] |
| Destination buffer to receive the public key of the mcuxClEls_EccKeyGen_Async operation. More... | |
| static mcuxClEls_EccByte_t | ecc_public_key_server [MCUXCLELS_ECC_PUBLICKEY_SIZE] |
| static uint8_t | derivation_data [MCUXCLELS_TLS_DERIVATIONDATA_SIZE] |
| static uint8_t | client_random [MCUXCLELS_TLS_RANDOM_SIZE] |
| static uint8_t | server_random [MCUXCLELS_TLS_RANDOM_SIZE] |
| static uint8_t | master_key_string [] |
| static uint8_t | key_expansion_string [] |
TLS key derivation example.
| MCUXCLEXAMPLE_FUNCTION | ( | mcuxClEls_Tls_Master_Key_Session_Keys_example | ) |
Performs key derivation for TLS protocol.
| MCUXCLEXAMPLE_OK | The example code completed successfully |
| MCUXCLEXAMPLE_ERROR | The example code failed |
Initialize ELS, Enable the ELS
< [in] The TLS derivation data
< [in] Desired key properties. Only mcuxClEls_KeyProp_t::upprot_priv and mcuxClEls_KeyProp_t::upprot_sec are used, the rest are ignored.
< [in] The index of the TLS pre-master key, which is overwritten with the master key
< [in] The TLS derivation data
< [in] Desired key properties. Only mcuxClEls_KeyProp_t::upprot_priv and mcuxClEls_KeyProp_t::upprot_sec are used, the rest are ignored.
< [in] The index of the TLS master key, which is overwritten with one of the session keys.
deleted keyIdxPrivClient keySlot
deleted keyIdxPrivServer keySlot
deleted i keySlot
|
static |
Destination buffer to receive the public key of the mcuxClEls_EccKeyGen_Async operation.