Constants for the mcuxClKey component. More...
#include <mcuxClConfig.h>Go to the source code of this file.
Macros | |
| #define | MCUXCLKEY_STATUS_OK |
| Key operation successful. More... | |
| #define | MCUXCLKEY_STATUS_ERROR |
| Error occured during Key operation. More... | |
| #define | MCUXCLKEY_STATUS_FAILURE |
| Failure during execution. More... | |
| #define | MCUXCLKEY_STATUS_INVALID_INPUT |
| Invalid input. More... | |
| #define | MCUXCLKEY_STATUS_FAULT_ATTACK |
| Fault attack detected. More... | |
| #define | MCUXCLKEY_STATUS_CRC_NOT_OK |
| CRC verification failed. More... | |
| #define | MCUXCLKEY_STATUS_NOT_SUPPORTED |
| Functionality not supported. More... | |
| #define | MCUXCLKEY_LOADSTATUS_NOTLOADED |
| Key not loaded. More... | |
| #define | MCUXCLKEY_LOADSTATUS_MEMORY |
| Key is loaded to memory. More... | |
| #define | MCUXCLKEY_LOADSTATUS_COPRO |
| Key is loaded to HW IP slot. More... | |
| #define | MCUXCLKEY_LOADSTATUS_KEEPLOADED |
| Do not flush the key after the operation (for Symmetric keys only) More... | |
| #define | MCUXCLKEY_ALGO_ID_AES |
| AES key. More... | |
| #define | MCUXCLKEY_ALGO_ID_RSA |
| RSA key. More... | |
| #define | MCUXCLKEY_ALGO_ID_ECC_SHWS_GFP |
| ECC key using Short Weierstrass Curve over GF(p) More... | |
| #define | MCUXCLKEY_ALGO_ID_ECC_SHWS_GF2M |
| ECC key using Short Weierstrass Curve over GF(2^m) More... | |
| #define | MCUXCLKEY_ALGO_ID_ECC_MONTDH |
| ECC key for MontDH key exchange scheme. More... | |
| #define | MCUXCLKEY_ALGO_ID_ECC_EDDSA |
| ECC key for EdDSA signature scheme. More... | |
| #define | MCUXCLKEY_ALGO_ID_HMAC |
| HMAC key. More... | |
| #define | MCUXCLKEY_ALGO_ID_SM4 |
| SM4 key. More... | |
| #define | MCUXCLKEY_ALGO_ID_SM2 |
| SM2 key. More... | |
| #define | MCUXCLKEY_ALGO_ID_ECC_SHWS_GFP_EPHEMERAL_CUSTOM |
| ECC key using Short Weierstrass Curve over GF(p) with ephemeral custom domain parameters. More... | |
| #define | MCUXCLKEY_ALGO_ID_ECC_SHWS_GFP_STATIC_CUSTOM |
| ECC key using Short Weierstrass Curve over GF(p) with static custom domain parameters. More... | |
| #define | MCUXCLKEY_ALGO_ID_ALGO_MASK |
| Mask for Algorithm. More... | |
| #define | MCUXCLKEY_ALGO_ID_SYMMETRIC_KEY |
| Symmetric key. More... | |
| #define | MCUXCLKEY_ALGO_ID_PUBLIC_KEY |
| Public key. More... | |
| #define | MCUXCLKEY_ALGO_ID_PRIVATE_KEY |
| Private key. More... | |
| #define | MCUXCLKEY_ALGO_ID_PRIVATE_KEY_CRT |
| Private RSA key in CRT format. More... | |
| #define | MCUXCLKEY_ALGO_ID_KEY_PAIR |
| Key pair. More... | |
| #define | MCUXCLKEY_ALGO_ID_PRIVATE_KEY_CRT_DFA |
| RSA key pair, with the private part in CRT format. More... | |
| #define | MCUXCLKEY_ALGO_ID_USAGE_MASK |
| Mask for Key Usage. More... | |
| #define | MCUXCLKEY_SIZE_NOTUSED |
| key length field is not used (e.g. ECC keys) More... | |
| #define | MCUXCLKEY_SIZE_128 |
| 128 bit key, size in bytes More... | |
| #define | MCUXCLKEY_SIZE_160 |
| 160 bit key, size in bytes More... | |
| #define | MCUXCLKEY_SIZE_192 |
| 192 bit key, size in bytes More... | |
| #define | MCUXCLKEY_SIZE_224 |
| 224 bit key, size in bytes More... | |
| #define | MCUXCLKEY_SIZE_256 |
| 256 bit key, size in bytes More... | |
| #define | MCUXCLKEY_SIZE_320 |
| 320 bit key, size in bytes More... | |
| #define | MCUXCLKEY_SIZE_384 |
| 348 bit key, size in bytes More... | |
| #define | MCUXCLKEY_SIZE_512 |
| 512 bit key, size in bytes More... | |
| #define | MCUXCLKEY_SIZE_521 |
| 521 bit key, size in bytes More... | |
| #define | MCUXCLKEY_SIZE_1024 |
| 1024 bit key, size in bits More... | |
| #define | MCUXCLKEY_SIZE_2048 |
| 2048 bit key, size in bits More... | |
| #define | MCUXCLKEY_SIZE_3072 |
| 3072 bit key, size in bits More... | |
| #define | MCUXCLKEY_SIZE_4096 |
| 4096 bit key, size in bits More... | |
| #define | MCUXCLKEY_SIZE_6144 |
| 6144 bit key, size in bits More... | |
| #define | MCUXCLKEY_SIZE_8192 |
| 8192 bit key, size in bits More... | |
| #define | MCUXCLKEY_SIZE_128_IN_WORDS |
| 128 bit key, size in words More... | |
| #define | MCUXCLKEY_SIZE_160_IN_WORDS |
| 160 bit key, size in words More... | |
| #define | MCUXCLKEY_SIZE_192_IN_WORDS |
| 192 bit key, size in words More... | |
| #define | MCUXCLKEY_SIZE_224_IN_WORDS |
| 224 bit key, size in words More... | |
| #define | MCUXCLKEY_SIZE_256_IN_WORDS |
| 256 bit key, size in words More... | |
| #define | MCUXCLKEY_SIZE_320_IN_WORDS |
| 320 bit key, size in words More... | |
| #define | MCUXCLKEY_SIZE_384_IN_WORDS |
| 348 bit key, size in words More... | |
| #define | MCUXCLKEY_SIZE_512_IN_WORDS |
| 512 bit key, size in words More... | |
| #define | MCUXCLKEY_SIZE_521_IN_WORDS |
| 521 bit key, size in words More... | |
| #define | MCUXCLKEY_SIZE_1024_IN_WORDS |
| 1024 bit key, size in words More... | |
| #define | MCUXCLKEY_SIZE_2048_IN_WORDS |
| 2048 bit key, size in words More... | |
| #define | MCUXCLKEY_SIZE_3072_IN_WORDS |
| 3072 bit key, size in words More... | |
| #define | MCUXCLKEY_SIZE_4096_IN_WORDS |
| 4096 bit key, size in words More... | |
| #define | MCUXCLKEY_SIZE_6144_IN_WORDS |
| 6144 bit key, size in words More... | |
| #define | MCUXCLKEY_SIZE_8192_IN_WORDS |
| 8192 bit key, size in words More... | |
| #define | MCUXCLKEY_WA_SIZE_MAX |
| Define the max workarea size required for this component. More... | |
| #define | MCUXCLKEY_INVALID_KEYSLOT |
| Define the value for an invalid key slot. More... | |
Constants for the mcuxClKey component.