Example for the mcuxClKey component. More...
#include <mcuxClKey.h>#include <mcuxClSession.h>#include <mcuxCsslFlowProtection.h>#include <mcuxClCore_FunctionIdentifiers.h>#include <mcuxClCore_Examples.h>#include <stdbool.h>#include <mcuxClAes.h>#include <mcuxClExample_Session_Helper.h>#include <mcuxClExample_Key_Helper.h>Functions | |
| MCUXCLEXAMPLE_FUNCTION (mcuxClKey_example) | |
| Performs an example initialization and cleanup of the mcuxClKey component. More... | |
Variables | |
| static uint32_t | aes128_key [MCUXCLAES_AES128_KEY_SIZE_IN_WORDS] |
Example for the mcuxClKey component.
| MCUXCLEXAMPLE_FUNCTION | ( | mcuxClKey_example | ) |
Performs an example initialization and cleanup of the mcuxClKey component.
| MCUXCLEXAMPLE_OK | The example code completed successfully |
| MCUXCLEXAMPLE_ERROR | The example code failed |
Destroy Session and cleanup Session