Top-level API of the mcuxClMac component. More...
#include <mcuxClConfig.h>#include <mcuxClSession_Types.h>#include <mcuxClKey_Types.h>#include <mcuxClMac_Types.h>#include <mcuxClCore_Platform.h>#include <mcuxClCore_Buffer.h>Go to the source code of this file.
Functions | |
| MCUX_CSSL_FP_PROTECTED_TYPE (mcuxClMac_Status_t) mcuxClMac_compute(mcuxClSession_Handle_t session | |
| One-shot message authentication code (MAC) computation function. More... | |
Variables | |
| mcuxClKey_Handle_t | key |
| mcuxClKey_Handle_t mcuxClMac_Mode_t | mode |
| mcuxClKey_Handle_t mcuxClMac_Mode_t mcuxCl_InputBuffer_t | pIn |
| mcuxClKey_Handle_t mcuxClMac_Mode_t mcuxCl_InputBuffer_t uint32_t | inLength |
| mcuxClKey_Handle_t mcuxClMac_Mode_t mcuxCl_InputBuffer_t uint32_t mcuxCl_Buffer_t | pMac |
| mcuxClKey_Handle_t mcuxClMac_Mode_t mcuxCl_InputBuffer_t uint32_t mcuxCl_Buffer_t uint32_t *const | pMacLength |
| mcuxClMac_Context_t *const | pContext |
Top-level API of the mcuxClMac component.