Type definitions for the mcuxClMac component. More...
#include <stdint.h>#include <stdbool.h>#include <stddef.h>#include <mcuxClConfig.h>#include <mcuxClSession_Types.h>#include <mcuxCsslFlowProtection.h>#include <mcuxClCore_FunctionIdentifiers.h>Go to the source code of this file.
Typedefs | |
| typedef uint32_t | mcuxClMac_Status_t |
| Type for Mac component error codes. More... | |
| typedef struct mcuxClMac_ModeDescriptor | mcuxClMac_ModeDescriptor_t |
| MAC mode/algorithm descriptor type. More... | |
| typedef const mcuxClMac_ModeDescriptor_t *const | mcuxClMac_Mode_t |
| MAC mode/algorithm type. More... | |
| typedef mcuxClMac_ModeDescriptor_t *const | mcuxClMac_CustomMode_t |
| MAC custom mode/algorithm type. More... | |
| typedef struct mcuxClMac_Context | mcuxClMac_Context_t |
| Mac context type. More... | |
Type definitions for the mcuxClMac component.