Top-level API of the mcuxClSession component. More...
#include <mcuxClCore_Platform.h>#include <mcuxClCore_FunctionIdentifiers.h>#include <mcuxCsslFlowProtection.h>#include <mcuxClSession_Types.h>Go to the source code of this file.
Functions | |
| MCUX_CSSL_FP_PROTECTED_TYPE (mcuxClSession_Status_t) mcuxClSession_init(mcuxClSession_Handle_t pSession | |
| Initialize a Crypto Library session. More... | |
Variables | |
| uint32_t *const | pCpuWaBuffer |
| uint32_t *const uint32_t | cpuWaLength |
| uint32_t *const uint32_t uint32_t *const | pPkcWaBuffer |
| uint32_t *const uint32_t uint32_t *const uint32_t | pkcWaLength |
| uint8_t *const | pRtf |
| uint8_t *const mcuxClSession_Rtf_t | RtfOptions |
Top-level API of the mcuxClSession component.