Configuration of the implementation for the flow protection mechanism. More...
Go to the source code of this file.
Macros | |
| #define | MCUX_CSSL_FP_USE_CODE_SIGNATURE |
| If set to 1, use the flow protection mechanism implementation based on the Zen-V code signature HW mechanism. More... | |
| #define | MCUX_CSSL_FP_USE_SECURE_COUNTER |
| If set to 1, use the flow protection mechanism implementation based on the CSSL secure counter mechanism. More... | |
| #define | MCUX_CSSL_FP_USE_NONE |
| If set to 1, do not use the flow protection mechanism. More... | |
Configuration of the implementation for the flow protection mechanism.