header file of memory set function More...
#include <stdint.h>#include <stddef.h>#include <mcuxCsslFlowProtection.h>#include <mcuxCsslFlowProtection_FunctionIdentifiers.h>#include <mcuxCsslParamIntegrity.h>Go to the source code of this file.
Functions | |
| MCUX_CSSL_FP_PROTECTED_TYPE (mcuxCsslMemory_Status_t) mcuxCsslMemory_Set(mcuxCsslParamIntegrity_Checksum_t chk | |
Set length bytes of data at pDst. More... | |
Variables | |
| void * | pDst |
| void uint8_t | val |
| void uint8_t size_t | length |
| void uint8_t size_t size_t | bufLength |
header file of memory set function