Provides the API for the CSSL secure counter mechanism. More...
#include <mcuxCsslSecureCounter_Impl.h>Go to the source code of this file.
Macros | |
| #define | MCUX_CSSL_SC_CHECK_PASSED |
| Positive comparison result value. More... | |
| #define | MCUX_CSSL_SC_CHECK_FAILED |
| Negative comparison result value. More... | |
| #define | MCUX_CSSL_SC_VALUE_TYPE |
| Data type used for the secure counter values. More... | |
| #define | MCUX_CSSL_SC_ALLOC() |
| Allocation operation for the secure counter. More... | |
| #define | MCUX_CSSL_SC_INIT(value) |
| Initialization operation for the secure counter. More... | |
| #define | MCUX_CSSL_SC_CHECK(reference) |
| Comparison operation for the secure counter. More... | |
| #define | MCUX_CSSL_SC_ADD(value) |
Increment the secure counter with value. More... | |
| #define | MCUX_CSSL_SC_ADD_ON_CALL(value) |
Increment the secure counter with value in case of function call. More... | |
| #define | MCUX_CSSL_SC_ADD_0x1() |
| Increment the secure counter with 0x1. More... | |
| #define | MCUX_CSSL_SC_ADD_0x10() |
| Increment the secure counter with 0x10. More... | |
| #define | MCUX_CSSL_SC_ADD_0x100() |
| Increment the secure counter with 0x100. More... | |
| #define | MCUX_CSSL_SC_SUB(value) |
Decrement the secure counter with value. More... | |
| #define | MCUX_CSSL_SC_SUB_0x1() |
| Decrement the secure counter with 0x1. More... | |
| #define | MCUX_CSSL_SC_SUB_0x10() |
| Decrement the secure counter with 0x10. More... | |
| #define | MCUX_CSSL_SC_SUB_0x100() |
| Decrement the secure counter with 0x100. More... | |
| #define | MCUX_CSSL_SC_VALUE() |
| Access operation for the current secure counter value. More... | |
| #define | MCUX_CSSL_SC_ASSIGN(value) |
| Assignment operation for the secure counter. More... | |
Provides the API for the CSSL secure counter mechanism.