Parameter structure for function #mcuxClEcc_Verify. More...
#include <mcuxClEcc_Types.h>
Data Fields | |
| mcuxClEcc_DomainParam_t | curveParam |
| [in] structure of pointers to curve parameters and length of parameters. More... | |
| const uint8_t * | pPrecG |
| [in] pointer to octet string of pre-computed point of base point G, which is of the same format as base point G. More... | |
| const uint8_t * | pHash |
| [in] pointer to string of message digest (hash), of which the length is byteLenHash (in optLen). More... | |
| const uint8_t * | pSignature |
| [in] pointer to octet string of signature R and S. More... | |
| const uint8_t * | pPublicKey |
| [in] pointer to octet string of public key, which is of the same format as base point G. More... | |
| uint8_t * | pOutputR |
| [out] pointer to memory area in which signature R calculated by verify function will be exported if signature is valid. More... | |
| uint32_t | optLen |
| [in] packed options (reserved) and lengths: bits 0~7: byteLenHash: length of the string of message digest; bits 8~31: reserved. More... | |
Parameter structure for function #mcuxClEcc_Verify.
| mcuxClEcc_DomainParam_t mcuxClEcc_Verify_Param_t::curveParam |
[in] structure of pointers to curve parameters and length of parameters.
| const uint8_t* mcuxClEcc_Verify_Param_t::pPrecG |
[in] pointer to octet string of pre-computed point of base point G, which is of the same format as base point G.
It is calculated as (2 ^ (nByteLength * 4)) * G.
| const uint8_t* mcuxClEcc_Verify_Param_t::pHash |
[in] pointer to string of message digest (hash), of which the length is byteLenHash (in optLen).
| const uint8_t* mcuxClEcc_Verify_Param_t::pSignature |
[in] pointer to octet string of signature R and S.
Each of R and S is a Big-endian octet string of the exact length curveParam.byteLenN. The string of R is followed by the string of S.
| const uint8_t* mcuxClEcc_Verify_Param_t::pPublicKey |
[in] pointer to octet string of public key, which is of the same format as base point G.
| uint8_t* mcuxClEcc_Verify_Param_t::pOutputR |
[out] pointer to memory area in which signature R calculated by verify function will be exported if signature is valid.
It will be stored as a Big-endian octet string of the exact length curveParam.byteLenN.
| uint32_t mcuxClEcc_Verify_Param_t::optLen |
[in] packed options (reserved) and lengths: bits 0~7: byteLenHash: length of the string of message digest; bits 8~31: reserved.