Command option bit field for #mcuxClEls_Cmac_Async. More...
#include <mcuxClEls_Cmac.h>
Data Fields | |
| struct { | |
| uint32_t value | |
| Accesses the bit field as a full word. More... | |
| } | word |
| Access mcuxClEls_CmacOption_t word-wise. More... | |
| struct { | |
| uint32_t initialize: 1 | |
| Request initial processing for the first block of the message. More... | |
| uint32_t finalize: 1 | |
| Request final processing for the last block of the message. More... | |
| uint32_t soe: 1 | |
| This field is managed internally. More... | |
| uint32_t sie: 1 | |
| This field is managed internally. More... | |
| uint32_t __pad0__:9 | |
| RFU. More... | |
| uint32_t extkey:1 | |
| An external key should be used. More... | |
| uint32_t __pad1__:18 | |
| RFU. More... | |
| } | bits |
| Access mcuxClEls_CmacOption_t bit-wise. More... | |
Command option bit field for #mcuxClEls_Cmac_Async.
| uint32_t mcuxClEls_CmacOption_t::value |
Accesses the bit field as a full word.
| struct { ... } mcuxClEls_CmacOption_t::word |
Access mcuxClEls_CmacOption_t word-wise.
| uint32_t mcuxClEls_CmacOption_t::initialize |
Request initial processing for the first block of the message.
| uint32_t mcuxClEls_CmacOption_t::finalize |
Request final processing for the last block of the message.
| uint32_t mcuxClEls_CmacOption_t::soe |
This field is managed internally.
| uint32_t mcuxClEls_CmacOption_t::sie |
This field is managed internally.
| uint32_t mcuxClEls_CmacOption_t::__pad0__ |
RFU.
| uint32_t mcuxClEls_CmacOption_t::extkey |
An external key should be used.
| uint32_t mcuxClEls_CmacOption_t::__pad1__ |
RFU.
| struct { ... } mcuxClEls_CmacOption_t::bits |
Access mcuxClEls_CmacOption_t bit-wise.