| ► examples | |
| mcuxCl_clns.h | CLNS header for component-independent functionality |
| mcuxClAead.h | Top-level include file for the mcuxClAead component |
| mcuxClAead_Constants.h | Constants for use with the mcuxClAead component |
| mcuxClAead_Functions.h | Top-level API of the mcuxClAead component |
| mcuxClAead_Types.h | Type definitions for the mcuxClAead component |
| mcuxClAeadModes.h | |
| mcuxClAeadModes_MemoryConsumption.h | |
| mcuxClAeadModes_Modes.h | |
| mcuxClAes.h | Top-level interface header for the mcuxClAes component |
| mcuxClAes_Constants.h | |
| mcuxClAes_KeyTypes.h | Definition of supported key types in mcuxClAes component, see also mcuxClKey component |
| mcuxClCipher.h | Top-level include file for the mcuxClCipher component |
| mcuxClCipher_Constants.h | Constants for use with the mcuxClCipher component |
| mcuxClCipher_Functions.h | Top-level API of the mcuxClCipher component |
| mcuxClCipher_Types.h | Type definitions for the mcuxClCipher component |
| mcuxClCipherModes.h | |
| mcuxClCipherModes_MemoryConsumption.h | |
| mcuxClCipherModes_Modes.h | Supported modes for the mcuxClCipher component |
| mcuxClCore_Analysis.h | |
| mcuxClCore_Buffer.h | |
| mcuxClCore_Examples.h | |
| mcuxClCore_FunctionIdentifiers.h | Definition of function identifiers for the flow protection mechanism |
| mcuxClCore_Platform.h | |
| mcuxClCore_Toolchain.h | |
| mcuxClEcc.h | Top level header of mcuxClEcc component |
| mcuxClEcc_Constants.h | Constants definition for domain parameters of supported curves |
| mcuxClEcc_Functions.h | Top level APIs of mcuxClEcc component |
| mcuxClEcc_KeyMechanisms.h | ECC related definitions to be used for key handling mechanisms of the mcuxClKey component |
| mcuxClEcc_MemoryConsumption.h | Defines the memory consumption for the mcuxClEcc component |
| mcuxClEcc_ParameterSizes.h | Definitions of ECC domain parameter, key and signature sizes |
| mcuxClEcc_Types.h | Type definitions of mcuxClEcc component |
| mcuxClEcc_WeierECC.h | Header of mcuxClEcc functionalities related to ECC protocols based on (short) Weierstrass curves |
| mcuxClEls.h | Top-level include file for the ELS driver |
| mcuxClEls_Aead.h | ELS header for Authenticated Encryption with Associated Data (AEAD) |
| mcuxClEls_Cipher.h | ELS header for symmetric ciphers |
| mcuxClEls_Cmac.h | ELS header for CMAC support |
| mcuxClEls_Common.h | ELS header for common functionality |
| mcuxClEls_Crc.h | ELS header for Command CRC functionality |
| mcuxClEls_Ecc.h | ELS header for elliptic curve cryptography This header exposes functions that enable using the ELS for elliptic curve cryptography |
| mcuxClEls_Hash.h | ELS header for hashing |
| mcuxClEls_Hmac.h | ELS header for HMAC support |
| mcuxClEls_Kdf.h | ELS header for key derivation |
| mcuxClEls_KeyManagement.h | ELS header for key management |
| mcuxClEls_mapping.h | Header providing mapping for legacy function/definition names (with CSS) |
| mcuxClEls_Rng.h | ELS header for random number generation |
| mcuxClEls_Types.h | ELS type header |
| mcuxClExample_ELS_Helper.h | |
| mcuxClExample_ELS_Key_Helper.h | |
| mcuxClExample_Key_Helper.h | |
| mcuxClExample_RFC3394_Helper.h | |
| mcuxClExample_RNG_Helper.h | |
| mcuxClExample_Session_Helper.h | |
| mcuxClHash.h | Top-level include file for the mcuxClHash component |
| mcuxClHash_Algorithms.h | Algorithm/mode definitions for the mcuxClHash component |
| mcuxClHash_Constants.h | Constants for use with the mcuxClHash component |
| mcuxClHash_Functions.h | Top-level API of the mcuxClHash component |
| mcuxClHash_MemoryConsumption.h | Defines the memory consumption for the mcuxClHash component |
| mcuxClHash_Types.h | Type definitions for the mcuxClHash component |
| mcuxClKey.h | Top-level include file for the mcuxClKey component |
| mcuxClKey_Constants.h | Constants for the mcuxClKey component |
| mcuxClKey_Functions.h | Top-level API of the mcuxClKey component |
| mcuxClKey_KeyTypes.h | Definition of supported key types in mcuxClKey component |
| mcuxClKey_MemoryConsumption.h | |
| mcuxClKey_ProtectionMechanisms.h | |
| mcuxClKey_Types.h | Type definitions for the mcuxClKey component |
| mcuxClMac.h | Top-level include file for the mcuxClMac component |
| mcuxClMac_Constants.h | Constants and status codes for the mcuxClMac component |
| mcuxClMac_Functions.h | Top-level API of the mcuxClMac component |
| mcuxClMac_Types.h | Type definitions for the mcuxClMac component |
| mcuxClMacModes.h | |
| mcuxClMacModes_Constants.h | Constants for the mcuxClMacModes component |
| mcuxClMacModes_Functions.h | Functions for the mcuxClMacModes component |
| mcuxClMacModes_MemoryConsumption.h | Defines the memory consumption for the mcuxClMacModes component All work area sizes in bytes are a multiple of CPU wordsize |
| mcuxClMacModes_Modes.h | |
| mcuxClMath.h | Top level header of mcuxClMath component |
| mcuxClMath_Functions.h | APIs of mcuxClMath component |
| mcuxClMath_Types.h | |
| mcuxClMemory.h | Top-level include file for the memory operations |
| mcuxClMemory_Clear.h | Memory header for clear functions |
| mcuxClMemory_Copy.h | Memory header for copy functions |
| mcuxClMemory_Endianness.h | Memory header for endianness support functions |
| mcuxClMemory_Set.h | Memory header for set function |
| mcuxClMemory_Types.h | Memory type header |
| mcuxClOscca_FunctionIdentifiers.h | Definition of function identifiers for the flow protection mechanism |
| mcuxClOscca_Memory.h | : Macros for alignment memory |
| mcuxClOscca_PlatformTypes.h | : Platform type definitions |
| mcuxClOscca_Types.h | : Global type definitions |
| mcuxClOsccaPkc.h | Top level header of mcuxClOsccaPkc component (PKC hardware driver) |
| mcuxClOsccaPkc_Functions.h | APIs of mcuxClOsccaPkc component |
| mcuxClOsccaPkc_Types.h | Type definitions of mcuxClOsccaPkc component |
| mcuxClOsccaSm3.h | Top-level include file for the mcuxClOsccaSm3 component |
| mcuxClOsccaSm3_Algorithms.h | Algorithm/mode definitions for the mcuxClOsccaSm3 component |
| mcuxClOsccaSm3_Constants.h | Constants for use with the mcuxClOsccaSm3 component |
| mcuxClOsccaSm3_MemoryConsumption.h | Defines the memory consumption for the mcuxClOsccaSm3 component |
| mcuxClPadding.h | Top-level include file for the padding component |
| mcuxClPadding_Constants.h | Constants definitions for the mcuxClPadding component |
| mcuxClPadding_Types.h | Type definitions for the mcuxClPadding component |
| mcuxClPkc.h | Top level header of mcuxClPkc component (PKC hardware driver) |
| mcuxClPkc_Functions.h | APIs of mcuxClPkc component |
| mcuxClPkc_Types.h | Type definitions of mcuxClPkc component |
| mcuxClRandom.h | Top level header of mcuxClRandom component |
| mcuxClRandom_Constants.h | Constant definitions of mcuxClRandom component |
| mcuxClRandom_Functions.h | Top level APIs of mcuxClRandom component |
| mcuxClRandom_Types.h | Type definitions of mcuxClRandom component |
| mcuxClRandomModes.h | Top level header of mcuxClRandomModes component |
| mcuxClRandomModes_Constants.h | Mode definitions of mcuxClRandomModes component |
| mcuxClRandomModes_Functions_PatchMode.h | |
| mcuxClRandomModes_Functions_TestMode.h | |
| mcuxClRandomModes_MemoryConsumption.h | Defines the memory consumption for the mcuxClRandom component |
| mcuxClRsa.h | Top-level include file for the mcuxClRsa component |
| mcuxClRsa_Constants.h | Constant definitions for the mcuxClRsa component |
| mcuxClRsa_Functions.h | Top-level API of the mcuxClRsa component |
| mcuxClRsa_MemoryConsumption.h | Defines the memory consumption for the mcuxClRsa component |
| mcuxClRsa_Types.h | Type definitions for the mcuxClRsa component |
| mcuxClSession.h | Top-level include file for the mcuxClSession component |
| mcuxClSession_Functions.h | Top-level API of the mcuxClSession component |
| mcuxClSession_Types.h | Type definitions for the mcuxClSession component |
| mcuxCsslAnalysis.h | |
| mcuxCsslCPreProcessor.h | The default implementation is based on standard C preprocessor functionality |
| mcuxCsslFlowProtection.h | Provides the API for the CSSL flow protection mechanism |
| mcuxCsslFlowProtection_Cfg.h | Configuration of the implementation for the flow protection mechanism |
| mcuxCsslFlowProtection_FunctionIdentifiers.h | Definition of function identifiers for the flow protection mechanism |
| mcuxCsslFlowProtection_Impl.h | Selection of the implementation for the flow protection mechanism |
| mcuxCsslFlowProtection_SecureCounter_Common.h | Counter based implementation for the flow protection mechanism, for a local security counter |
| mcuxCsslFlowProtection_SecureCounter_Local.h | Counter based implementation for the flow protection mechanism, for a local security counter |
| mcuxCsslMemory.h | Top-level include file for the CSSL memory functions |
| mcuxCsslMemory_Clear.h | Header file of memory clear function |
| mcuxCsslMemory_Compare.h | Include file for constant time memory compare function |
| mcuxCsslMemory_Copy.h | Include file for memory copy function |
| mcuxCsslMemory_Set.h | Header file of memory set function |
| mcuxCsslMemory_Types.h | Type definitions for the mcuxCsslMemory component |
| mcuxCsslParamIntegrity.h | Top-level include file for the parameter integrity protection mechanism |
| mcuxCsslSecureCounter.h | Provides the API for the CSSL secure counter mechanism |
| mcuxCsslSecureCounter_Cfg.h | Configuration of the implementation for the secure counter mechanism |
| mcuxCsslSecureCounter_Impl.h | Selection of the implementation for the secure counter mechanism |
| mcuxCsslSecureCounter_None.h | Implementation that disables the CSSL secure counter mechanism |
| mcuxCsslSecureCounter_SW_Local.h | SW implementation of the CSSL secure counter mechanism (using a local variable) |