Defines all macros of mcuxClEls_Types. More...
Modules | |
| MCUXCLELS_KEYPROPERTY_VALUE_ | |
| Constants for initalizing mcuxClEls_KeyProp_t.word. | |
| MCUXCLELS_KEYPROPERTY_ | |
| Constants for initalizing mcuxClEls_KeyProp_t.bits. | |
| MCUXCLELS_STATUS_ | |
| Return code definitions. | |
Macros | |
| #define | MCUXCLELS_KEY_SLOTS |
| Number of key slots in the ELS key store. More... | |
| #define | MCUXCLELS_STATUS_IS_HW_ERROR(x) |
| Checks whether an error code is a hardware error. Indicates that an error was reported by ELS hardware. More... | |
| #define | MCUXCLELS_STATUS_IS_SW_ERROR(x) |
| Checks whether an error code is a software error. Indicates that the error was detected by the driver software and not by ELS hardware. More... | |
Defines all macros of mcuxClEls_Types.
| #define MCUXCLELS_KEY_SLOTS |
Number of key slots in the ELS key store.
| #define MCUXCLELS_STATUS_IS_HW_ERROR | ( | x | ) |
Checks whether an error code is a hardware error. Indicates that an error was reported by ELS hardware.
| #define MCUXCLELS_STATUS_IS_SW_ERROR | ( | x | ) |
Checks whether an error code is a software error. Indicates that the error was detected by the driver software and not by ELS hardware.