Example for the mcuxClEcc component. More...
#include <mcuxClCore_Examples.h>#include <mcuxClSession.h>#include <mcuxClCore_FunctionIdentifiers.h>#include <mcuxClExample_Session_Helper.h>#include <mcuxClKey.h>#include <mcuxClEcc.h>#include <mcuxClEcc_WeierECC.h>#include <mcuxCsslFlowProtection.h>Macros | |
| #define | BN256_BYTE_LEN_P |
| #define | BN256_BYTE_LEN_N |
| #define | MAX_CPUWA_SIZE |
| #define | MAX_PKCWA_SIZE |
Functions | |
| MCUXCLEXAMPLE_FUNCTION (mcuxClEcc_WeierECC_CustomEccWeierType_BN256_example) | |
| Performs an example key derivation using the mcuxClKey component. More... | |
Example for the mcuxClEcc component.
| MCUXCLEXAMPLE_FUNCTION | ( | mcuxClEcc_WeierECC_CustomEccWeierType_BN256_example | ) |
Performs an example key derivation using the mcuxClKey component.
| MCUXCLEXAMPLE_OK | The example code completed successfully |
| MCUXCLEXAMPLE_ERROR | The example code failed |