: Platform type definitions More...
#include <stdint.h>#include <stddef.h>#include <stdbool.h>#include <platform_specific_headers.h>Go to the source code of this file.
Data Structures | |
| struct | mcuxClOscca_ScratchPad_t |
| global scratch pad structure definition More... | |
Macros | |
| #define | MCUX_CLOSCCA_SCRATCHPAD_SECTION |
Typedefs | |
| typedef uint32_t | mcuxClOscca_Size_t |
| typedef uint32_t | mcuxClOscca_Uint_t |
| typedef int32_t | mcuxClOscca_Int_t |
Variables | |
| mcuxClOscca_ScratchPad_t MCUX_CLOSCCA_SCRATCHPAD_SECTION | gmcuxClOscca_ScratchPad |
| global scratch pad object More... | |
: Platform type definitions
| mcuxClOscca_ScratchPad_t MCUX_CLOSCCA_SCRATCHPAD_SECTION gmcuxClOscca_ScratchPad |
global scratch pad object