Example of ECC for key generation, signing and verification using the ELS (CLNS component mcuxClEls) More...
#include <mcuxClEls.h>#include <mcuxCsslFlowProtection.h>#include <mcuxClCore_FunctionIdentifiers.h>#include <mcuxClCore_Examples.h>#include <mcuxClExample_ELS_Helper.h>#include <mcuxClExample_ELS_Key_Helper.h>Functions | |
| MCUXCLEXAMPLE_FUNCTION (mcuxClEls_Ecc_Keygen_Sign_Verify_example) | |
| Performs SHA2-256 hashing using mcuxClEls functions. More... | |
Variables | |
| static uint32_t const | ecc_digest [MCUXCLELS_HASH_OUTPUT_SIZE_SHA_256/sizeof(uint32_t)] |
| Pre-hashed data to be signed. More... | |
| static uint32_t | ecc_public_key [MCUXCLELS_ECC_PUBLICKEY_SIZE/sizeof(uint32_t)] |
| Destination buffer to receive the public key of the mcuxClEls_EccKeyGen_Async operation. More... | |
| static mcuxClEls_EccByte_t | ecc_signature [MCUXCLELS_ECC_SIGNATURE_SIZE] |
| Destination buffer to receive the signature of the mcuxClEls_EccSign_Async operation. More... | |
| static mcuxClEls_EccByte_t | ecc_signature_r [MCUXCLELS_ECC_SIGNATURE_R_SIZE] |
| Destination buffer to receive the signature part r of the VerifyOptions operation. More... | |
| static mcuxClEls_EccByte_t | ecc_signature_and_public_key [MCUXCLELS_ECC_SIGNATURE_SIZE+MCUXCLELS_ECC_PUBLICKEY_SIZE] |
| Concatenation of the ECC signature and public key, needed for the mcuxClEls_EccVerify_Async operation. More... | |
Example of ECC for key generation, signing and verification using the ELS (CLNS component mcuxClEls)
| MCUXCLEXAMPLE_FUNCTION | ( | mcuxClEls_Ecc_Keygen_Sign_Verify_example | ) |
Performs SHA2-256 hashing using mcuxClEls functions.
| MCUXCLEXAMPLE_OK | The example code completed successfully |
| MCUXCLEXAMPLE_ERROR | The example code failed |
Initialize ELS, Enable the ELS
deleted keyIdx keySlot
Disable the ELS
|
static |
Pre-hashed data to be signed.
|
static |
Destination buffer to receive the public key of the mcuxClEls_EccKeyGen_Async operation.
|
static |
Destination buffer to receive the signature of the mcuxClEls_EccSign_Async operation.
|
static |
Destination buffer to receive the signature part r of the VerifyOptions operation.
|
static |
Concatenation of the ECC signature and public key, needed for the mcuxClEls_EccVerify_Async operation.