ELS header for controlling the glitch detector. More...
Go to the source code of this file.
Macros | |
| #define | MCUXCLELS_GLITCHDETECTOR_CFG_SIZE |
| Glitch detector configuration size. More... | |
| #define | MCUXCLELS_GLITCHDETECTOR_TRIM_SIZE |
| Glitch detector trim value size. More... | |
Functions | |
| MCUXCLELS_API | MCUX_CSSL_FP_PROTECTED_TYPE (mcuxClEls_Status_t) mcuxClEls_GlitchDetector_LoadConfig_Async(uint8_t const *pInput) |
| Loads a glitch detector configuration. More... | |
ELS header for controlling the glitch detector.
This header exposes functions that configure the ELS glitch detector.