This file includes defines, enums and typedefs for decoder elements.
More...
|
| #define | DECODER_INTERLEAVED false |
| | Decoder interleaved. More...
|
| |
|
#define | DECODER_NONINTERLEAVED true |
| | Decoder noninterleaved.
|
| |
|
#define | DECODER_SIGNED true |
| | Decoder signed.
|
| |
|
#define | DECODER_UNSIGNED false |
| | Decoder unsigned.
|
| |
|
| enum | DecoderOutputWordLength {
DECODER_OUTPUT_WORD_LENGTH_8 = 8
,
DECODER_OUTPUT_WORD_LENGTH_16 = 16
,
DECODER_OUTPUT_WORD_LENGTH_24 = 24
,
DECODER_OUTPUT_WORD_LENGTH_32 = 32
,
LAST_DECODER_OUTPUT_WORD_LENGTH
} |
| |
|
| int32_t | decoder_init_element (StreamElement *element) |
| | This function initializes the decoder element, and loads the pad source and sink functions. More...
|
| |
| int32_t | decoder_change_state (StreamElement *element, PipelineState new_dec_state) |
| | This function changes the decoder state by calling STATE_TRANSITION pipeline macro. If the new state is NULL_TO_READY, it verifies the decoder type is known and handler is setup. More...
|
| |
| uint32_t | decoder_get_duration (ElementDecoder *element, StreamDataFormat data) |
| | Returns the duration of a source PadQueryFunc is called to return the element duration in the format defined by the StreamDataFormat parameter. More...
|
| |
| void | decoder_set_duration (ElementDecoder *element, uint32_t stream_size, uint32_t bit_rate) |
| | Calculate and set the duration of a source This function calculates the duration in bytes using the stream size and stream bitrate, and sets it in bytes in the ElementDecoder variable. More...
|
| |
| int32_t | decoder_set_property (StreamElement *element, uint16_t prop_id, uint32_t prop_value) |
| | Set a property of a decoder element. More...
|
| |
| int32_t | decoder_get_property (StreamElement *element, uint16_t prop_id, uint32_t *prop_value) |
| | Get a property of a decoder element. More...
|
| |
| int32_t | decoder_set_type (ElementHandle element, DecoderType dec_type) |
| | Set the decoder type for the input element. This function maps the generic decoder element pad handlers to the specific decoder implementation using DecoderHandlersType. More...
|
| |
| int32_t | decoder_activate_parse_tag (ElementHandle element, uint8_t activate) |
| | Enable/Disable the tag parsing Sets the parse_tag variable to the value passed in via activate variable. More...
|
| |
| bool | decoder_is_source_seekable (ElementDecoder *decoder, StreamDataFormat format) |
| | Is current source seekable. More...
|
| |
| void | vUpdateAverageBitrate (ElementDecoder *element) |
| | Update a running average of bit rate. More...
|
| |
◆ DECODER_INTERLEAVED
| #define DECODER_INTERLEAVED false |
Buffer sizes for supported decoders
◆ DecoderOutputWordLength
The decoder output word length
◆ decoder_init_element()
| int32_t decoder_init_element |
( |
StreamElement * |
element | ) |
|
◆ decoder_change_state()
| int32_t decoder_change_state |
( |
StreamElement * |
element, |
|
|
PipelineState |
new_dec_state |
|
) |
| |
- Parameters
-
| element | StreamElement will be used to create ElementDecoder |
| new_dec_state | new decoder state to change to |
- Return values
-
| STREAM_ERR_INVALID_ARGS | invalid parameters |
| STREAM_ERR_GENERAL | if moved to ready state and decoders not setup |
| STREAM_OK | successful |
◆ decoder_get_duration()
| uint32_t decoder_get_duration |
( |
ElementDecoder * |
element, |
|
|
StreamDataFormat |
data |
|
) |
| |
- Parameters
-
| element | ElementDecoder pointer will be used to create StreamPad sink |
| data | StreamDataFormat defines the format of the data to return. |
- Returns
- duration or 0 if failed
◆ decoder_set_duration()
| void decoder_set_duration |
( |
ElementDecoder * |
element, |
|
|
uint32_t |
stream_size, |
|
|
uint32_t |
bit_rate |
|
) |
| |
- Parameters
-
| element | ElementDecoder pointer will hold the calculated duration value |
| stream_size | Size of the stream |
| bit_rate | Bit rate of the stream |
- Returns
- None
◆ decoder_set_property()
| int32_t decoder_set_property |
( |
StreamElement * |
element, |
|
|
uint16_t |
prop_id, |
|
|
uint32_t |
prop_value |
|
) |
| |
This is a new interface to replace the original decoder_set_type().
- Parameters
-
| element | StreamElement pointer |
| prop_id | id number of a element's property |
| prop_value | the property value to be set |
- Returns
- StreamReturnType
- Return values
-
| STREAM_OK | if successful |
| STREAM_ERR_INVALID_ARGS | means invalid arguments |
◆ decoder_get_property()
| int32_t decoder_get_property |
( |
StreamElement * |
element, |
|
|
uint16_t |
prop_id, |
|
|
uint32_t * |
prop_value |
|
) |
| |
- Parameters
-
| element | StreamElement pointer that will be used as ElementHandle |
| prop_id | id number of a element's property |
| prop_value | the property value to be saved in |
- Return values
-
| STREAM_OK | if successful |
| STREAM_ERR_INVALID_ARGS | means invalid arguments |
◆ decoder_set_type()
- Parameters
-
| element | ElementHandle that will be used as ElementDecoder to set the handlers to the input decoder type |
| dec_type | DecoderType value that will be used to map the appropriate handler functions. |
- Return values
-
| STREAM_OK | if successful |
| STREAM_ERR_INVALID_ARGS | means invalid arguments |
| STREAM_ERR_GENERAL | is returned if dec_type is not handled |
◆ decoder_activate_parse_tag()
| int32_t decoder_activate_parse_tag |
( |
ElementHandle |
element, |
|
|
uint8_t |
activate |
|
) |
| |
- Parameters
-
| element | ElementHandle that will be used as ElementDecoder |
| activate | value used to set parse_tag in decoder element. |
- Return values
-
| STREAM_OK | if successful |
| STREAM_ERR_INVALID_ARGS | means invalid arguments |
◆ decoder_is_source_seekable()
| bool decoder_is_source_seekable |
( |
ElementDecoder * |
decoder, |
|
|
StreamDataFormat |
format |
|
) |
| |
This function sends a query to sink pad of the decoder element to check if check if seek is possible in the specified format.
- Parameters
-
| decoder | ElementDecoder pointer will be use to create a sink StreamPad |
| format | format type used to create the query. |
- Returns
- bool
- Return values
-
| true | source is seekable |
| false | souce is not seekable |
◆ vUpdateAverageBitrate()
| void vUpdateAverageBitrate |
( |
ElementDecoder * |
element | ) |
|
- Parameters
-
| element | ElementDecoder pointer that will contain the calculated average bit rate. |
- Returns
- None