|
| void | FILE_Dump_Task (void *param) |
| | this function is a task that writes data to the SD card More...
|
| |
| static uint8_t | filesink_sink_pad_activation_handler (StreamPad *pad, uint8_t active) |
| | This function activates the sink pad and allocates memory for the file sink element. More...
|
| |
| static FlowReturn | filesink_sink_pad_chain_handler (StreamPad *pad, StreamBuffer *buf) |
| | This pad function accumulates data from the decoder and pushes it onto the selected audio driver. The audio sink maintains a double buffer and starts sending data once both the buffers are full. It blocks if the previous data is not sent out by the driver for some reason. More...
|
| |
| static int32_t | filesink_sink_pad_process_handler (StreamPad *pad) |
| | File sink pad process handler. More...
|
| |
| static uint8_t | filesink_sink_pad_event_handler (StreamPad *pad, StreamEvent *event) |
| | This function is the calls the specified audio device driver implementation of the sink pad event handler. More...
|
| |
| static int32_t | filesink_change_state (StreamElement *element, PipelineState new_state) |
| | This function changes the file sink state and calls the appropriate apis for that state and takes the actions and then returns. PipelineState Transition: NULL to READY: Open file READY to PAUSE: Activate sink pads and their peer pads PAUSE to PLAY: Start Writing PAUSE to READY: Deactivate sink pads and their peer pads READY to NULL: Close file. More...
|
| |
| static uint8_t | filesink_sink_pad_query_handler (StreamPad *pad, StreamQuery *query) |
| | This pad function handles query from the pipeline. If not able to handle the query then it pushes the query to its peer. More...
|
| |
| static int32_t | filesink_set_property (StreamElement *element_ptr, uint16_t prop, uint32_t val) |
| | This function sets audio sink element's properties. More...
|
| |
| static int32_t | filesink_get_property (StreamElement *element_ptr, uint16_t prop, uint32_t *val_ptr) |
| | This function gets audio sink element's properties. More...
|
| |
| int32_t | filesink_init_element (StreamElement *element) |
| | this function initializes the audio sink element and sink pads More...
|
| |
| int32_t | filesink_set_location (ElementHandle element, char *path) |
| | This function sets a destiniaiton file to be writen by file sink. More...
|
| |
| int32_t | filesink_set_write_mode (ElementHandle element, uint8_t write_mode) |
| | Set the raw write mode or the packet header mode to write to file. More...
|
| |