This file includes defines, enums and typedefs for memory sink.
More...
|
| int32_t | memsink_set_buffer (ElementHandle element_hdl, char *location_ptr, uint32_t size) |
| | Set the location of the memory buffer to write to as well as the size. More...
|
| |
| int32_t | memsink_set_raw_write_mode (ElementHandle element_hdl, uint8_t raw_write_mode) |
| | This function sets the raw write mode or the packet header mode to write to memory. (write_mode == true) means only data will be written (no packet headers) (write_mode == false) means packet header will be written aOSA_LONG with data. More...
|
| |
| int32_t | memsink_init_element (StreamElement *element_ptr) |
| | This function initializes the memory sink element and sink pads. More...
|
| |
◆ memsink_set_buffer()
| int32_t memsink_set_buffer |
( |
ElementHandle |
element_hdl, |
|
|
char * |
location_ptr, |
|
|
uint32_t |
size |
|
) |
| |
- Parameters
-
| element_hdl | element handle |
| location_ptr | location path |
| size | memory buffer size |
- Returns
- StreamReturnType
- Return values
-
| STREAM_OK | success |
| STREAM_ERR_INVALID_ARGS | invalid parameters |
| STREAM_ERR_GENERAL | status is bigger than or eque to STATE_PAUSED |
◆ memsink_set_raw_write_mode()
| int32_t memsink_set_raw_write_mode |
( |
ElementHandle |
element_hdl, |
|
|
uint8_t |
raw_write_mode |
|
) |
| |
- Parameters
-
| element_hdl | element handle |
| raw_write_mode | write mode raw (or) packet header |
- Returns
- StreamReturnType
- Return values
-
| STREAM_OK | success |
| STREAM_ERR_INVALID_ARGS | invalid arguments |
| STREAM_ERR_GENERAL | value is bigger than or eque to STATE_PAUSED |
◆ memsink_init_element()
| int32_t memsink_init_element |
( |
StreamElement * |
element_ptr | ) |
|
- Parameters
-
| element_ptr | pointer of memory sink element instance |
- Returns
- StreamReturnType
- Return values
-
| STREAM_OK | success |
| STREAM_ERR_ELEMENT_NOT_FOUND | invalid instance pointer of element_ptr |