Implements a data ringbuffer.
More...
#include <string.h>
#include "ringbuffer.h"
#include "fsl_os_abstraction.h"
◆ ringbuf_create()
| ringbuf_t * ringbuf_create |
( |
uint32_t |
size | ) |
|
- Parameters
-
| size | Buffer size to be malloc'd |
- Returns
- Initialized and allocated pointer to ring buffer object
◆ ringbuf_destroy()
| void ringbuf_destroy |
( |
ringbuf_t * |
rb | ) |
|
- Parameters
-
| rb | Pointer to ring buffer object created with ringbuf_create |
◆ ringbuf_clear()
| void ringbuf_clear |
( |
ringbuf_t * |
rb | ) |
|
- Parameters
-
| rb | Pointer to ring buffer object created with ringbuf_create |
◆ ringbuf_get_occupancy()
| uint32_t ringbuf_get_occupancy |
( |
ringbuf_t * |
rb | ) |
|
- Parameters
-
| rb | Pointer to ring buffer object created with ringbuf_create |
- Returns
- Number of bytes of data currently occupying space in the buffer
◆ ringbuf_write()
| uint32_t ringbuf_write |
( |
ringbuf_t * |
rb, |
|
|
uint8_t * |
data, |
|
|
uint32_t |
size |
|
) |
| |
- Parameters
-
| rb | Pointer to ring buffer object created with ringbuf_create |
| data | Input buffer of data to write to ring buffer |
| size | Number of bytes to write to ring buffer, from 'data' |
- Returns
- Number of bytes successfully written to buffer
◆ _ringbuf_read_internal()
| static uint32_t _ringbuf_read_internal |
( |
ringbuf_t * |
rb, |
|
|
uint8_t * |
data, |
|
|
uint32_t |
size, |
|
|
bool |
peek |
|
) |
| |
|
static |
- Parameters
-
| rb | Pointer to ringbuffer structure |
| data | Data pointer |
| size | Size to be read |
| peek | Flag for moving ringbuffer head |
- Returns
- uint32_t
◆ ringbuf_read()
| uint32_t ringbuf_read |
( |
ringbuf_t * |
rb, |
|
|
uint8_t * |
data, |
|
|
uint32_t |
size |
|
) |
| |
- Parameters
-
| rb | Pointer to ring buffer object created with ringbuf_create |
| data | Output buffer of data to write from ring buffer. Can be NULL, in which case data is discarded. |
| size | Number of bytes to read from ring buffer, to store in 'data' |
- Returns
- Number of bytes successfully read to buffer or discarded
◆ ringbuf_peek()
| uint32_t ringbuf_peek |
( |
ringbuf_t * |
rb, |
|
|
uint8_t * |
data, |
|
|
uint32_t |
size |
|
) |
| |
- Parameters
-
| rb | Pointer to ring buffer object created with ringbuf_create |
| data | Output buffer of data to write from ring buffer. |
| size | Number of bytes to read from ring buffer, to store in 'data' |
- Returns
- Number of bytes successfully read to buffer