![]() |
Maestro Audio Framework v 1.5
NXP Semiconductors
|
This file includes definitions for messages used by the Streamer library. More...
Macros | |
| #define | BLD_MESSAGE(msg, type) ((uint32_t)(((uint32_t)(msg) << 24) | ((uint32_t)(type)))) |
| Build a message. More... | |
| #define | MESSAGE_ID(msg) (uint32_t)((msg) >> 24) |
| Get message ID. | |
| #define | MESSAGE_TYPE(msg) (uint32_t)((msg)&0xFFF) |
| Get message type. | |
| #define | MSG_NULL (uint32_t)0 |
| Null message. | |
| #define | MSG_EOS BLD_MESSAGE(MESSAGE_EOS, 0) |
| End of stream message from the pipeline. | |
| #define | MSG_ERROR_AUDIO BLD_MESSAGE(MESSAGE_ERROR, ERROR_AUDIO_FATAL) |
| Actual error type will be decoder dependent passed on in message data field. | |
| #define | MSG_WARNING_AUDIO BLD_MESSAGE(MESSAGE_ERROR, WARNING_AUDIO) |
| Actual warning type will be decoder dependent passed on in message data field. | |
| #define | MSG_INFO_AUDIO_BITRATE BLD_MESSAGE(MESSAGE_INFO, INFO_AUDIO_BITRATE) |
| Message data will contain the bitrate in bits per second. | |
| #define | MSG_INFO_AUDIO_CHANNELS BLD_MESSAGE(MESSAGE_INFO, INFO_AUDIO_CHANNELS) |
| Message data will contain the number of channels supported. | |
| #define | MSG_INFO_AUDIO_SAMPLERATE BLD_MESSAGE(MESSAGE_INFO, INFO_AUDIO_SAMPLERATE) |
| Message data will contain the audio sampling rate in Hz. | |
| #define | MSG_INFO_AUDIO_TYPE BLD_MESSAGE(MESSAGE_INFO, INFO_AUDIO_TYPE) |
| Message data will contain the type of audio. Audio type depends on the decoders supported. | |
| #define | MSG_INFO_CODEC_INFO BLD_MESSAGE(MESSAGE_INFO, INFO_CODEC_INFO) |
| Message data will contain the pointer to a string of codec info. | |
| #define | MSG_INFO_DURATION BLD_MESSAGE(MESSAGE_INFO, INFO_DURATION) |
| Message data will contain the total duration of playback in milliseconds. | |
| #define | MSG_INFO_ALBUM BLD_MESSAGE(MESSAGE_INFO, INFO_ALBUM) |
| Nothing in message data. get tag function should be called to get the required tag. | |
| #define | MSG_INFO_ARTIST BLD_MESSAGE(MESSAGE_INFO, INFO_ARTIST) |
| Nothing in message data. get tag function should be called to get the required tag. | |
| #define | MSG_INFO_TITLE BLD_MESSAGE(MESSAGE_INFO, INFO_TITLE) |
| Nothing in message data. get tag function should be called to get the required tag. | |
| #define | MSG_INFO_GENRE BLD_MESSAGE(MESSAGE_INFO, INFO_GENRE) |
| Nothing in message data. get tag function should be called to get the required tag. | |
| #define | MSG_INFO_YEAR BLD_MESSAGE(MESSAGE_INFO, INFO_YEAR) |
| Nothing in message data. get tag function should be called to get the required tag. | |
| #define | MSG_INFO_TRACK BLD_MESSAGE(MESSAGE_INFO, INFO_TRACK) |
| Nothing in message data. get tag function should be called to get the required tag. | |
| #define | MSG_INFO_ALBUMART BLD_MESSAGE(MESSAGE_INFO, INFO_ALBUMART_IMAGE) |
| Message data will contain the total duration of playback in milliseconds. | |
| #define | MSG_INFO_POSITION BLD_MESSAGE(MESSAGE_INFO, INFO_POSITION) |
| Message data will contain the current time of playback in milliseconds. | |
| #define | MSG_STREAM_INFO_UPDATED BLD_MESSAGE(MESSAGE_INFO, INFO_STREAM_INFO_UPDATE) |
| Nothing in message data. indicate that all stream information is updated. | |
| #define | MSG_META_INFO_UPDATED BLD_MESSAGE(MESSAGE_INFO, INFO_META_INFO_UPDATE) |
| Nothing in message data. indicate that all metadata information is updated. | |
| #define | MSG_STREAM_ERROR BLD_MESSAGE(MESSAGE_INFO, INFO_ERROR) |
| Message data will contain the error type. | |
| #define BLD_MESSAGE | ( | msg, | |
| type | |||
| ) | ((uint32_t)(((uint32_t)(msg) << 24) | ((uint32_t)(type)))) |
| msg | Message id |
| type | message type |
Max ID of message is 8. Each ID can have 24 types. Bits 31-24: Message ID Bits 23-0: Message type