![]() |
Maestro Audio Framework v 1.5
NXP Semiconductors
|
#include <pipeline.h>
Data Fields | |
| PipelineState | state |
| Current Pipeline State. | |
| unsigned int | index |
| Pipeline Index within Streamer Task. | |
| osa_msgq_handle_t * | app_mq |
| Application Message Queue. | |
| StreamElement | level_head [MAX_ELEMENT_LEVEL] |
| Element Head Array. | |
| StreamPipelineType | type |
| the pipeline type | |
| bool | repeat |
| should pipeline play current stream repeatedly | |
| TrackInfo | track_info |
| Track info cached. | |
Pipeline Pipeline object structure