Overview - pmsm_periph_framework example
========================================
This example demonstrates pins and peripherals setting, which can be used as a template for motor control application.
Note, that motor spinning is not available by default in this example - example does not contain state machines and motor control algorithms.

Hardware requirements
=====================
- Micro USB cable
- LPCXpresso55S36-EVK board
- Personal Computer
- FRDM-MC-LVPMSM board (optional)

Toolchain supported
===================
- IAR embedded Workbench  9.40.1
- Keil MDK  5.38
- MCUXpresso IDE 11.8.0

Prepare the example
===================
1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board.
2. Download the program to the target board.
3. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
4. Open pmsm_periph_framework.pmxm file. Navigate to 'Project -> Options -> MAP files' and search for the generated symbol file.
5. Click 'Start communication'. Observe and edit available variables in the 'Variable Watch'.

Initialized peripherals
=======================
- CTimer - used to generate the slow-loop interrupt
- eFlexPWM - used for 6-channel PWM generation
- ADC - used for phase currents and DC-bus voltage measurement
- HSCMP - used for DC-bus over-current detection
- INPUTMUX - used for signal routing
- Flexcomm - used for serial communication with the FreeMASTER tool

Functionality
=============
- Enable/disable PWM outputs
- Update PWM registers value
- Measure phase currents and DC-bus voltage
- DC-bus over-current fault detection
- Monitor and visualization data using FreeMASTER tool (use pmsm_periph_framework.pmxm file)

More information
================
- Application web page: https://www.nxp.com/sdkmotorcontrol.