Overview
========
The 3-phase permanent magnet synchronous motor (PMSM) control reference application 
is  intended to provide the example for 3-phase PMSM motor control solutions. 
The reference design uses a closed-loop field-oriented vector speed (FOC) control mechanism.

More information
================
- Release note is in SDK install folder\docs\MC\Release_notes.pdf.
- Application User's guide is in SDK install folder\docs\MC\*.pdf.
- Application web page: http://www.nxp.com/sdkmotorcontrol.

Running the demo
================
- Follow chapters "Hardware setup" and "User interface" in Application User's guide.