![]() |
eRPC API Reference
Rev. 1.11.0
NXP Semiconductors
|
This is the complete list of members for erpc::Crc16, including all inherited members.
| computeCRC16(const uint8_t *data, uint32_t lengthInBytes) | erpc::Crc16 | |
| Crc16(uint32_t crcStart) | erpc::Crc16 | explicit |
| Crc16(void) | erpc::Crc16 | |
| m_crcStart | erpc::Crc16 | protected |
| setCrcStart(uint32_t crcStart) | erpc::Crc16 | |
| ~Crc16(void) | erpc::Crc16 |